2024-08-07 6:55 AM
I'm trying to boot from SD-card and u-boot doesn't seem to find device tree. I have built my system with buildroot (bootlin st/2023.02.2) overriding the sources for tf-a, u-boot, op-tee and kernel, to be able to boot at least to u-boot (I did write another posts of my problems).
The files in SD-card
boot
├── extlinux
│ └── extlinux.conf
├── myb-stm32mp135x-512m.dtb
└── zImage
extlinux.conf
label myb-stm32mp135x-512m-buildroot
kernel /boot/zImage
devicetree /boot/myb-stm32mp135x-512m.dtb
append root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200
genimage
image sdcard.img {
hdimage {
partition-table-type = "gpt"
}
partition fsbl1 {
image = "%ATFBIN%"
}
partition fsbl2 {
image = "%ATFBIN%"
}
partition fip {
image = "fip.bin"
}
partition u-boot-env {
size = 2M
}
partition rootfs {
image = "rootfs.ext4"
bootable = "yes"
}
}
So any ideas why it doesn't work?
2024-08-07 7:00 AM
I forgot to add the boot log
Boot over mmc0!
Saving Environment to MMC... Writing to redundant MMC(0)... OK
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:5...
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
Scanning disk mmc@58005000.blk...
Scanning disk mmc@58007000.blk...
Found 16 disks
No EFI system partition
Error: eth2@5800e000 address not set.
Error: eth1@5800a000 address not set.
Error: eth2@5800e000 address not set.
Error: eth1@5800a000 address not set.
spi-nand: spi_nand MT29F2G01AB@0: unknown raw ID daf51a88
Device spi-nand0 not found!
ETZPC: 0x5a003000 node disabled, decprot 6=1
FDT: cryp@54002000 node disabled for STM32MP135D Rev.Y
BootOrder not defined
EFI boot manager: Cannot load any image
2024-09-19 3:29 AM - edited 2024-09-19 3:30 AM
Hi,
were you able to solve your problem? I having similar issue.
2024-09-20 12:29 AM
Hi,
please have a look to https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command ?
Regards.
2024-09-28 4:09 AM
Thanks a lot, Patrick. This worked for formatting the SD card. But I had some changed configuration, because of that It could not boot to linux. I changed my configuration, and from u-boot console I gave some boot command and after that, and it booted through Linux. Thanks again.