2023-07-05 1:06 PM
Hello, In order to use the non-default QSPI boot locations, my understanding is port0-port3, 4 signals need to be defined in OTP words 3, 5, and 6 based on a similar question about SDMMC1 discussed here:
https://community.st.com/t5/stm32-mpu-products/how-to-change-emmc-interface/td-p/344994
For QSPI the default signals according to the getting started guide, AN5474, are:
PB2 QUADSPI_BK1_NCSQUADSPI_BK1_NCS
PF10 QUADSPI_CLK
PF8 QUADSPI_BK1_IO0
PF9 QUADSPI_BK1_IO1
What is the mapping for the OTP ports 0-3 to the functional signal names NCS, CLK, IO0, IO1?
i.e. port 0=NCS, CLK, IO0, or IO1? Same for the other three ports.
I was not able to find this described or an example for QSPI and OTP.
Thanks.
Solved! Go to Solution.
2023-07-24 12:51 AM
Hi @Jasper
no order, BootROM blindly apply all OTP5, 6 and 7 content.
It is possible to define whatever you want, up to 6 pins. Anyway, for QSPI Boot point of view only CLK, CMD, IO0 and IO1 are required.
As soon as OTP3 define to use non-default pins for QSPI, BootROM does not map anymore the default pins for CLK, CMD, IO0 and IO1.
IO2 and IO3 would never be set nor used by BootROM, so no risk of any conflict.
Note: some Serial memories can use IO2 and IO3 pins as additional feature such as hold. To
enable such device to boot, it might be necessary to set those pins to inactive level by adding external pull-ups or by defining internal pull-up during Boot using OTP7.
For later boot stage, you need to define your full QSPI pinmux in uBoot Device Tree which will override those used by BootROM.
Regarding you chosen pins, to enable the boot, you would need :
Please double check these values according to your need and https://wiki.st.com/stm32mpu/wiki/STM32MP13_OTP_mapping#AFmux_configuration
Regards.
2023-07-10 6:56 AM
Also, think I need the OTP port number mapping for QUAD SPI IO2 and IO3.
2023-07-21 8:57 AM - edited 2023-07-21 9:03 AM
HI @Jasper
you need to define
If you give the non-default pins you require, I can provide to you a set of values for OTPs.
like this (useless) example for:
would need:
See also https://wiki.st.com/stm32mpu/wiki/STM32MP13_OTP_mapping#AFmux_configuration
Regards.
2023-07-23 2:11 PM
Hi Patrick.
Is there any particular order these signals need to be defined in CFG's?
For example could I start with IO0 then IO1 in CFG5 and then CLK then CS in CF6 or is this not valid?
Also, is it possible to define all 6 non default pins by using CFG7.
The default IO2 and IO3 would be connected to some hardware other than the QSPI device.
I don't know if the ROM code would drive the default IO2 and IO3 to some value during ROM boot.
Thanks.
The non-default pins I'm considering:
PD4 - QUADSPI_CLK, AF9 |
PE14 - QUADSPI_BK1 _NCS, AF9 |
PD5 - QUADSPI_BK1_IO0, AF9 |
PE9 - QUADSPI_BK1 _IO1, AF9 |
PD11 - QUADSPI_BK1_IO2, AF9 |
PD15 - QUADSPI_BK1_IO3, AF9 |
2023-07-24 12:51 AM
Hi @Jasper
no order, BootROM blindly apply all OTP5, 6 and 7 content.
It is possible to define whatever you want, up to 6 pins. Anyway, for QSPI Boot point of view only CLK, CMD, IO0 and IO1 are required.
As soon as OTP3 define to use non-default pins for QSPI, BootROM does not map anymore the default pins for CLK, CMD, IO0 and IO1.
IO2 and IO3 would never be set nor used by BootROM, so no risk of any conflict.
Note: some Serial memories can use IO2 and IO3 pins as additional feature such as hold. To
enable such device to boot, it might be necessary to set those pins to inactive level by adding external pull-ups or by defining internal pull-up during Boot using OTP7.
For later boot stage, you need to define your full QSPI pinmux in uBoot Device Tree which will override those used by BootROM.
Regarding you chosen pins, to enable the boot, you would need :
Please double check these values according to your need and https://wiki.st.com/stm32mpu/wiki/STM32MP13_OTP_mapping#AFmux_configuration
Regards.