2021-07-13 2:22 AM
currently i have a pin <STM32_PINMUX('F', 14, GPIO)> how to mux as a GPIO before using as a gpiolib, export work fine, but i2c4 is not working but i can see GPIO is getting based on sys gpiolib.
as before export i see PF14 line is muxed as pin 94 (PF14): input - low - pull up
and this line has AF as a i2c4-clk
2021-07-15 7:17 AM
Hi Ara.1 (Community Member)
I am not sure to understand what you try to acheive here. if you've declared PF14 as AF assigned to i2c4-clk, the i2c driver will use this pin (pinctrl framework). This is mutually exclusive to control PF14 as a GPIO using gpiolib framework.
Maybe a good starting point: https://wiki.st.com/stm32mpu/wiki/Overview_of_GPIO_pins
Regards,
Olivier
2021-07-15 8:44 AM
point 1
echo 94 > /sys/class/gpio/export -
point 2
gpioset gpiochip5 14=1
2021-07-15 8:52 AM
Hi Ara.1 (Community Member)
Understood...
sysfs gpio is deprecated since Linux 4.8, you should use gpiochip instead.
BR
Olivier
2021-07-15 11:00 AM
sysfs gpio i can set and reset, same reflecting on PF14, but why i2c4 lines are different touch is failing this looks strange.
2021-07-21 8:23 AM
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'