SPL Initialize Error on DDR Ram speed
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-04 8:10 AM
Hello,
I am trying to bring up a custom board based on the STM32MP157D MPU via SDCard.
I am using u-boot 2022-01-rc3 as bootloader and the boot is using SPL (I have an SDCard with a GPT Partition table with fsbl1, fsbl2 and ssbl named partitions).
This is the 2nd time I am using this u-boot to bring up a custom STM32MP15x board.
The first time was using a STM32MP151a and I needed to activate the clock tree for the USART1 and modified the low level setup in the stm32mp1_clk source code to enable the USART1 clocks and to activate the serial port #1 to have the SPL ready to print as soon it starts.
But now, something goes wrong. I am using a DDR3 layout as the ED1 evaluation kit as 2x4GB (2x16 bit) 533Mhz DDR RAM. Using the same clk initialization stuff in the ddr3-1066-888-bin-g-2x4gb-533mhz device tree file, and the rcc configuration as follow:
&rcc {
status = "okay";
st,clksrc = <
CLK_MPU_PLL1P
CLK_AXI_PLL2P
CLK_MCU_PLL3P
CLK_PLL12_HSE
CLK_PLL3_HSE
CLK_PLL4_HSE
CLK_RTC_LSE
CLK_MCO1_DISABLED
CLK_MCO2_DISABLED
>;
st,clkdiv = <
1 /*MPU*/
0 /*AXI*/
0 /*MCU*/
1 /*APB1*/
1 /*APB2*/
1 /*APB3*/
1 /*APB4*/
2 /*APB5*/
23 /*RTC*/
0 /*MCO1*/
0 /*MCO2*/
>;
st,pkcs = <
CLK_CKPER_HSE
CLK_FMC_ACLK
CLK_QSPI_ACLK
CLK_ETH_DISABLED
CLK_SDMMC12_PLL4P
CLK_DSI_DSIPLL
CLK_STGEN_HSE
CLK_USBPHY_HSE
CLK_SPI2S1_PLL3Q
CLK_SPI2S23_PLL3Q
CLK_SPI45_HSI
CLK_SPI6_HSI
CLK_I2C46_HSI
CLK_SDMMC3_PLL4P
CLK_USBO_USBPHY
CLK_ADC_CKPER
CLK_CEC_LSE
CLK_I2C12_HSI
CLK_I2C35_HSI
CLK_UART1_HSI
CLK_UART24_HSI
CLK_UART35_HSI
CLK_UART6_HSI
CLK_UART78_HSI
CLK_SPDIF_PLL4P
CLK_FDCAN_PLL4R
CLK_SAI1_PLL3Q
CLK_SAI2_PLL3Q
CLK_SAI3_PLL3Q
CLK_SAI4_PLL3Q
CLK_RNG1_LSI
CLK_RNG2_LSI
CLK_LPTIM1_PCLK1
CLK_LPTIM23_PCLK3
CLK_LPTIM45_LSE
>;
/* VCO = 1066.0 MHz => P = 266 (AXI), Q = 533 (GPU), R = 533 (DDR) */
pll2: st,pll@1 {
compatible = "st,stm32mp1-pll";
reg = <1>;
cfg = < 2 65 1 0 0 PQR(1,1,1) >;
frac = < 0x1400 >;
u-boot,dm-pre-reloc;
};
/* VCO = 417.8 MHz => P = 209, Q = 24, R = 11 */
pll3: st,pll@2 {
compatible = "st,stm32mp1-pll";
reg = <2>;
cfg = < 1 33 1 16 36 PQR(1,1,1) >;
frac = < 0x1a04 >;
u-boot,dm-pre-reloc;
};
/* VCO = 594.0 MHz => P = 99, Q = 74, R = 74 */
pll4: st,pll@3 {
compatible = "st,stm32mp1-pll";
reg = <3>;
cfg = < 3 98 5 7 7 PQR(1,1,1) >;
u-boot,dm-pre-reloc;
};
};
it fails with:
U-Boot SPL 2022.01-rc3 (Aug 04 2022 - 17:01:02 +0200)
RAM: EK470 DDR3-DDR3L 32bits 533000kHz
stm32mp1_clk rcc@50000000: stm32mp1_clk_disable: id clock 228 has been disabled
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 220 has been enabled
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 222 has been enabled
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 226 has been enabled
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 229 has been enabled
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 224 has been enabled
id=15 clock = 1fc4ef40 : 533000 kHz
stm32mp1_clk rcc@50000000: computed rate for id clock 224 is 533000000 (parent is PLL2_R)
stm32mp1_clk rcc@50000000: stm32mp1_clk_enable: id clock 228 has been enabled
get_ram_size(c0000000, 40000000)
info.size: 4
DDR invalid size : 0x4, expected 0x40000000
DRAM init failed: -22
### ERROR ### Please RESET the board ###
I suppose the ddr3 setup file in u-boot dts is using the right setup of memory (as the ed1 board I suppose it is working fine), so I cannot understand why the get_ram_size() function returns a single 32 bit (4 bytes) size.
Can help you out to jump over this issue?
Can be a wrong voltage on the DRAM chips?
Regards,
Gianluca
- Labels:
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-04 8:16 AM
as far as I know the vdd_ddr: buck2 is 1350000 microvolts 1.35V in the device-tree configuration of the STPMIC2APQR.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-05 2:25 AM
Just checked. VDD_DDR (despite the Buck2In is present (5VCC)) is 0V. This should explain the wrong DDR Calculation. Maybe it needs a working SDRAM chip ofcourse.
Now the REGULATORS is defined in the config:
CONFIG_PINCONF=y
# CONFIG_SPL_PINCTRL_FULL is not set
CONFIG_PINCTRL_STMFX=y
CONFIG_DM_PMIC=y
# CONFIG_SPL_PMIC_CHILDREN is not set
CONFIG_PMIC_STPMIC1=y
CONFIG_DM_REGULATOR=y
CONFIG_DM_REGULATOR_FIXED=y
CONFIG_DM_REGULATOR_GPIO=y
CONFIG_DM_REGULATOR_STM32_VREFBUF=y
CONFIG_DM_REGULATOR_STPMIC1=y
as well as the i2c4 setup (pinmux and i2c core) in the device tree:
&pinctrl_z {
u-boot,dm-pre-reloc;
i2c4_pins_z_mx: i2c4_mx-0 {
pins {
pinmux = <STM32_PINMUX('Z', 4, AF6)>, /* I2C4_SCL */
<STM32_PINMUX('Z', 5, AF6)>; /* I2C4_SDA */
bias-disable;
drive-open-drain;
slew-rate = <0>;
};
};
i2c4_sleep_pins_z_mx: i2c4_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('Z', 4, ANALOG)>, /* I2C4_SCL */
<STM32_PINMUX('Z', 5, ANALOG)>; /* I2C4_SDA */
};
};
The same is applied to the i2c4 bus controller:
&i2c4 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c4_pins_z_mx>;
pinctrl-1 = <&i2c4_sleep_pins_z_mx>;
i2c-scl-rising-time-ns = <185>;
i2c-scl-falling-time-ns = <20>;
clock-frequency = <100000>;
status = "okay";
/* spare dmas for other usage */
/delete-property/dmas;
/delete-property/dma-names;
pmic: stpmic@33 {
compatible = "st,stpmic1";
reg = <0x33>;
interrupts-extended = <&gpioa 0 IRQ_TYPE_EDGE_FALLING>;
interrupt-controller;
#interrupt-cells = <2>;
status = "okay";
regulators {
compatible = "st,stpmic1-regulators";
buck1-supply = <&vin>;
buck2-supply = <&vin>;
buck3-supply = <&vin>;
buck4-supply = <&vin>;
ldo1-supply = <&v3v3>;
ldo2-supply = <&vin>;
ldo3-supply = <&vdd_ddr>;
ldo4-supply = <&vin>;
ldo5-supply = <&vin>;
ldo6-supply = <&v3v3>;
vref_ddr-supply = <&vin>;
boost-supply = <&vin>;
pwr_sw1-supply = <&bst_out>;
pwr_sw2-supply = <&bst_out>;
vddcore: buck1 {
regulator-name = "vddcore";
regulator-min-microvolt = <1200000>;
regulator-max-microvolt = <1350000>;
regulator-always-on;
regulator-initial-mode = <0>;
regulator-over-current-protection;
};
vdd_ddr: buck2 {
regulator-name = "vdd_ddr";
regulator-min-microvolt = <1350000>;
regulator-max-microvolt = <1350000>;
regulator-always-on;
regulator-initial-mode = <0>;
regulator-over-current-protection;
};
vdd: buck3 {
regulator-name = "vdd";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
st,mask-reset;
regulator-initial-mode = <0>;
regulator-over-current-protection;
};
v3v3: buck4 {
regulator-name = "v3v3";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
regulator-over-current-protection;
regulator-initial-mode = <0>;
};
vtt_ddr: ldo3 {
regulator-name = "vtt_ddr";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
regulator-over-current-protection;
};
vdd_usb: ldo4 {
regulator-name = "vdd_usb";
interrupts = <IT_CURLIM_LDO4 0>;
};
vdda: ldo5 {
regulator-name = "vdda";
regulator-min-microvolt = <2900000>;
regulator-max-microvolt = <2900000>;
interrupts = <IT_CURLIM_LDO5 0>;
regulator-boot-on;
};
vref_ddr: vref_ddr {
regulator-name = "vref_ddr";
regulator-always-on;
};
bst_out: boost {
regulator-name = "bst_out";
interrupts = <IT_OCP_BOOST 0>;
};
vbus_otg: pwr_sw1 {
regulator-name = "vbus_otg";
interrupts = <IT_OCP_OTG 0>;
};
vbus_sw: pwr_sw2 {
regulator-name = "vbus_sw";
interrupts = <IT_OCP_SWOUT 0>;
regulator-active-discharge = <1>;
};
};
watchdog {
compatible = "st,stpmic1-wdt";
status = "disabled";
};
};
};
And, of course, the &i2c4 used in SPL and is enabled with: &i2c4{ u-boot,dm-pre-reloc; status="okay"; } as well as the &pinctrl_z { u-boot,dm-pre-reloc; status = "okay"; }
Even the pmic node is enabled in the SPL section with: &pmic { u-boot,dm-pre-reloc; status = "okay"; }
Is there a way to check (easely) with a scope, if the SPL is using the spl pmic driver *BEFORE* checking the RAM controller. It should be called as soon as possible during boot-up.
Do you agree with me?
Regards,
Gianluca
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-14 5:21 AM
Hi @gianlucarenzi​ ,
I read :
"u-boot 2022-01-rc3 as bootloader and the boot is using SPL"
Likely Vanilla U-boot version not yet integrated and ST no more support SPL for MP1.
I recommend you to use an OpenSTLinux delivery to get better support.
STM32 MPU OpenSTLinux release note - v4.0.0 - stm32mpu
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.