cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157 Device Tree ltdc port endpoint reg 0 vs reg 1

petero
Associate

Hi.

Some examples use ltdc_ep0_out / reg 0, while others use ltdc_ep1_out / reg 1.

e.g.

https://community.st.com/s/question/0D50X0000BG0RAWSQ3/stm32mp1-ltdc-device-tree-for-rgb-display

Where can I find more details on when to use reg 0 vs reg 1?

&ltdc {
	port {
		ltdc_ep1_out: endpoint@1 {
			reg = <1>;
			remote-endpoint = <&panel_rgb_in>;
		};
	};
};

Thank you

-- Peter

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Erwan SZYMANSKI
ST Employee

Hello @petero​ ,

Referring to the documentation (Documentation/devicetree/bindings/display/st,stm32-ltdc.yaml), you can find this information:

********************************************************

port:

$ref: /schemas/graph.yaml#/properties/port

description: |

Video port for DPI RGB output.

ltdc has one video port with up to 2 endpoints:

- for external dpi rgb panel or bridge, using gpios

- for internal dpi input of the MIPI DSI host controller

Note: These 2 endpoints cannot be activated simultaneously.

********************************************************

 It seems that the number linked with the endpoint has no impact on the DT, that is not the case with DSI for example.

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@petero​ ,

As a comparison, if the number of the port/endpoint has an impact, you will see the following thing in the yaml (example of Documentation/devicetree/bindings/display/st,stm32-dsi.yaml):

***************************************

ports:

$ref: /schemas/graph.yaml#/properties/ports

properties:

port@0:

$ref: /schemas/graph.yaml#/properties/port

description:

DSI input port node, connected to the ltdc rgb output port.

port@1:

$ref: /schemas/graph.yaml#/properties/port

description:

DSI output port node, connected to a panel or a bridge input port"

***************************************

Kind regards,

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.