2025-01-07 5:21 AM
Hello,
I'm trying to remove the packages which is not required to free up the memory.
I tried modifying the layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb file with the below code, But it couldn't help.
Here i tried to remove the alsa packag.
#To Disable the ALSA Package
IMAGE_INSTALL:remove = "\
alsa-conf \
alsa-plugins \
alsa-state \
alsa-state-script \
alsa-state-stm32mp1 \
alsa-states \
alsa-topology-conf \
alsa-ucm-conf \
alsa-utils \
alsa-utils-aconnect \
alsa-utils-alsabat \
alsa-utils-alsactl \
alsa-utils-alsaloop \
alsa-utils-alsamixer \
alsa-utils-alsatplg \
alsa-utils-alsaucm \
alsa-utils-amixer \
alsa-utils-aplay \
alsa-utils-aseqdump \
alsa-utils-aseqnet \
alsa-utils-iecset \
alsa-utils-midi \
alsa-utils-scripts \
alsa-utils-speakertest \
"
How can I remove the package.
Thanks and Regards,
Ezvan.
2025-01-07 5:56 AM - edited 2025-01-07 6:00 AM
Doing a grep:
grep -r alsa meta-st-stm32mp/
I can see that alsa is added to MACHINE_FEATURES in this file:
meta-st-stm32mp/conf/machine/include/st-machine-common-stm32mp.inc
in line:
MACHINE_FEATURES = "usbhost usbgadget alsa screen ext2 pci"
Maybe try removing it from here.
What is more, you shouldn't directly modify ST layer, the preffered way is to modify that MACHINE_FEATURES variable from your custom layer.
If that won't help, you can investigate it further using grep along with bitbake -e option, like that:
bitbake -e <your-image-name> | grep <what_to_search_for>
2025-01-22 4:40 PM
Hello @Ezvan
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Roger