2021-02-25 12:35 AM
Hello! I have just discovered that kit I would like to use to develop a new testing system within the company where I am working. However, I have some questions about it:
I truly thank you in advance for your answers!
Sincerely,
2021-03-09 01:16 AM
Hello @NAnt.3
In case you haven’t seen yet, some information can be found in the User Manual for the board on st.com
- Input voltage is only 5 V / 3 A USB Type-C™power supply input
- Available IO’s can be seen in the
◦ GPIO expansion connector (Raspberry Pi® shields capability)
◦ Arduino™ Uno V3 expansion connectors
Best Regards
JM