2021-04-19 11:01 PM
Hi,
I have been trying to flash the SD card of the STM32MP157A-DK1 following the instructions of the ST Wiki, although in this wiki the board used is the DK2. However the flashing process stops after a while and shows the errors that i attach in the pictures. The CubeProgrammer version is the 2.6. After some research i saw that another option could be execute the flashing process from the command shell but i have not been able to do it because it never finds the file to be flashed, despite copying it in the STM32CubeProgrammer\bin folder. Thanks in advance.
Solved! Go to Solution.
2021-04-21 01:42 AM
Hi,
I assume you are using W10 PC.
Once you have installed latest CubeProgrammer and downloaded/unzipped the starter package on a local folder,
Regards.
2021-04-21 01:42 AM
Hi,
I assume you are using W10 PC.
Once you have installed latest CubeProgrammer and downloaded/unzipped the starter package on a local folder,
Regards.
2021-04-22 12:12 AM
Thank you so much! This worked!