2021-12-17 3:27 AM
Hello,
I am using STM32mp157f-dk2 board and I have a peripheral connected on GPIO pin #16 ( PF1)
on doing gpoiget gpiochip5 1 > i get 1
on doing gpiosetgpiochip5 1=0 i DO NOT get any error but on doing again gpioget gpiochip5 1 > i get 1 again
I see it is shared with SDMMC3_CMD . On directly connecting it to Ground , it becomes low , not otherwise from the above commands.
Is this the same MMC on which starter image is written?Is it safe to pull it down permanently from the hardware?
May I know how to make it low from the software permanenetly.
Regards,D
Solved! Go to Solution.
2022-02-10 9:04 PM
Thanks @PatrickF This worked actually by following example code on stm32mpu wiki using the libgpiod example code :
Regards,
2022-01-04 12:36 AM
Hi @darla14 ,
may I suggest to try using devmem2 to directly access GPIO registers.
e.g.
# enable GPIOF IP clock in RCC
devmem2 0x50000A28 W 0x00000020
# set PF1 in GPIO output mode
# read the value (I read 0xBFBFFFCF on my DK2)
devmem2 0x50007000 W
# write the value modified with MODER1=0b01
devmem2 0x50007000 W 0xBFBFFFC7
# set PF1 = 0 using bit BR1 in GPIOF_BSRR (but PF1 should be already 0 as default value)
devmem2 0x50007018 W 0x00020000
Regards.
2022-01-04 12:45 AM
In fact, using "gpioget gpiochip5 1" will put PF1 in input mode (I assume you have an external pull-up as you read '1'), so should not be used after having issued "gpioset gpiochip5 1=0" which put PF1 in output with '0'.
Regards.
2022-02-10 9:04 PM
Thanks @PatrickF This worked actually by following example code on stm32mpu wiki using the libgpiod example code :
Regards,
2022-02-10 11:19 PM
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'