2024-12-28 6:00 AM
Hi,
When testing the stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.12.05 image, the LVDS screen doesn't work and blocks the board's startup (in u-boot) and I can't reset the board unless I disconnect the LVDS port.
On the other hand, the HDMI is functional, and the screen works without any problem on my STM32MP257F-EV1 board.
Note that the board is powered via a USB port capable of delivering up to 1.5A.
Thank you
2025-01-08 2:05 AM - edited 2025-01-08 2:06 AM
Hello @zakariazh ,
I've just tested the FlashLayout_sdcard_stm32mp257f-dk-ca35tdcid-ostl-m33-examples-optee.tsv on my board and the LVDS screen work fine.
Could you provide more information about your setup ? Do you have any trace to share ?
Best regard,