User Activity

Hi,When testing the stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.12.05 image, the LVDS screen doesn't work and blocks the board's startup (in u-boot) and I can't reset the board unless I disconnect the LVDS port.On the other hand, the HDMI is fun...
Hello,I have a STM32MP2 platform with A/B partitioning for TF-A, metadata and FIP.I'm looking for a way to generate a test FIP and install it in FIP-B bank, have TF-A load it, if this FIP contains a bad signature or other error that will prevent Uboo...
Hi,I am trying to boot a signed TF-A image on my STM32m257f compiled with TRUSTED_BOARD_BOOT support (Compiled in f-a-stm32mp.inc recipe from meta-st-stm32mp, mickledore branche).When the board is powered up, i got this error:  NOTICE: CPU: STM32MP2...
Hello,According to the doc, the Padding header extension adds the rest of the bytes in the header to complete the 512 bytes.When parsing a signed binary with STM32MP_SigningToolCLI, I find that the padding bytes have “random” values every time. Could...
Hello,I have 8 pairs of public and private keys with the hashes of each public key and I would like to calculate the associated PKHTH value without necessarily using the STM32MP_KeyGen_CLI tool (for integration with our manufacturing tool).I tried to...
Kudos from