cancel
Showing results for 
Search instead for 
Did you mean: 

Kernel panic during startup

uouox
Associate II

Hi I built the linux kernel by following the steps on the stm32mpu wiki web. All default configuration except enabled earlyprintk.

However, when I restart the system, it does not work any more.

This is the error in boot log.

...

[  0.349451] pps_core: LinuxPPS API ver. 1 registered

[  0.354493] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

[  0.363706] PTP clock support registered

[  0.368477] arm-scmi firmware:scmi0: SCMI Notifications - Core Enabled.

[  0.375147] 8<--- cut here ---

[  0.378218] Unhandled fault: external abort on non-linefetch (0x008) at 0xe081f004

[  0.385829] pgd = (ptrval)

[  0.388549] [e081f004] *pgd=c183c811, *pte=2ffff653, *ppte=2ffff453

[  0.394877] Internal error: : 8 [#1] PREEMPT SMP ARM

...

Any hint? The board is stm32mp157f-dk2

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @uouox​ ,

Could you please elaborate further if you used Developer package or Distribution package for rebuild ?

What ecosystem / kernel version ?

Are you using default Device Tree as per delivered by ST ?

Thx

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.