2025-05-07 9:56 PM - last edited on 2025-12-26 7:18 AM by ELABI.1
stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06.tar-gz from ECO 6.0 and only enabling the USB gadget drivers in .config, rebuilding the kernel and modules
The board freezes :
1. When the gadget driver is loaded and USB cable to host is plugged in
2. When the gadget driver is loaded w/o USB cable plugged in, the gadget is loaded and board does not freezen When plugging in the USB cable to the host, the board freezes.
Another vendor's 64 bit ARM board with kernel 6.6.xx does not freeze. Is there anything to debug with the device tree or otherwise to find the reason for lock up ?