2024-04-02 01:32 AM
Hi!
I was recommended to use the pre-built basic start-up projects for the STM32MP series, instead of buildning my own from scratch.
Solved: Re: Why are the DDR_DQ signals mixed in unsorted o... - STMicroelectronics Community
The project files are Altium Designer only, and I have Altium CircuitMaker. Is there any way to export these files into Altium CircuitMaker?
Solved! Go to Solution.
2024-05-24 05:13 AM
HI @DMårt
sorry for late reply.
I have asked internally, but it seems complex to provide PCB exports of reference design as we cannot easily check on our side that the export was not introducing mistakes.
Anyway, the point is taken to check if we could enhance that in future (but nothing in short term).
Regards.
2024-05-24 05:13 AM
HI @DMårt
sorry for late reply.
I have asked internally, but it seems complex to provide PCB exports of reference design as we cannot easily check on our side that the export was not introducing mistakes.
Anyway, the point is taken to check if we could enhance that in future (but nothing in short term).
Regards.
2024-05-26 03:39 AM - edited 2024-05-26 03:39 AM
It's working to export from Altium Designer to CircuitMaker. No problem there.
But I think CircuitMaker should be inclueded because CircuitMaker is very similar to Altium Designer. Almost copies.