cancel
Showing results for 
Search instead for 
Did you mean: 

is start the weston services must have the gpu support

Jzhua
Associate III

is stm32mp153 can start weston without gpu

3 REPLIES 3
Olivier GALLIEN
ST Employee

Hi @Jzhua​ 

Yes OpenSTLinux Weston can be used without GPU.

Using Distribution package if you reject the GCNANO licence agreement during configuration, you will have an automatic fallback to Weston display path not using GPU.

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

I just see the need to accept the eula. Do I need to say no? Like this

Do you accept the EULA you just read? (y/n) n
[WARNING] Configure build without support of packages under EULA acceptance.

Yes that's it.

Note that further adaptation may have to be done in the boot chain and Kernel Device Tree.

Using STM32CubeMX is recommended to help writing them.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.