2021-03-27 10:04 PM
I want to use stm32mp1 chip to drive ssd22288 rgb-mipi screen. Could you give me some solutions?
2021-03-28 12:45 AM
Only 157
The STM32MP1 series is available in 3 different lines which are pin-to-pin compatible:
STM32MP157: Dual Cortex-A7 cores up to @ 800 MHz, Cortex-M4 core @ 209 MHz, 3D GPU, DSI display interface and CAN FD
STM32MP153: Dual Cortex-A7 cores up to @ 800 MHz, Cortex-M4 core @ 209 MHz and CAN FD
STM32MP151: Single Cortex-A7 core up to @ 800 MHz, Cortex-M4 core @ 209 MHz