cancel
Showing results for 
Search instead for 
Did you mean: 

How to drive rgb-mipi screen

Wjian.1
Associate II

I want to use stm32mp1 chip to drive ssd22288 rgb-mipi screen. Could you give me some solutions?

1 REPLY 1
MM..1
Chief III

Only 157

The STM32MP1 series is available in 3 different lines which are pin-to-pin compatible:
STM32MP157: Dual Cortex-A7 cores up to @ 800 MHz, Cortex-M4 core @ 209 MHz, 3D GPU, DSI display interface and CAN FD
STM32MP153: Dual Cortex-A7 cores up to @ 800 MHz, Cortex-M4 core @ 209 MHz and CAN FD
STM32MP151: Single Cortex-A7 core up to @ 800 MHz, Cortex-M4 core @ 209 MHz