2022-01-28 1:41 PM
When I hit the build button, I get "Nothing to build for project DK2_TIMER1_OpenAmp_Solution", the Debug folder is also empty, should this be populated or do I need to generate it somehow?
https://www.youtube.com/watch?v=PsiFDHH87vo&list=PLnMKNibPkDnFeV4sBarnsAtFTg7h6V-9_&index=11
Solved! Go to Solution.
2022-02-15 9:30 AM
Hello @msche.1 ,
Sorry for the late reply.
I was finally able to work on your problem by installing the VM and trying to build.
I encountered the same issue than you by using the content described in the video.
The video was made with ecosystem 1.0.0 which is very old and with the tool STM32Workbench, which is now replaced by STM32CubeIDE, so the project syntax was different. That is why you were enable to build the project.
Procedure:
https://drive.google.com/drive/u/0/folders/1KQGGmHOE9Zq44O6KfNqAYMaGgkYwt42h
and download the folder "WorkshopUpdates_3_0_0-1.zip", which contains all the projects updated for the latest OSTL version.
Click on finish and select "DK2_TIMER1_OpenAmp_Solution_CM4" in the project explorer and click on the build icon (hammer):
You must be able to build the project.
If you want to do the other video, please keep in mind that the slides in the "WorkshopSlides" folder are the one up to date.
Hope it helps,
Regards,
Kévin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-01-31 9:11 AM
Hello @msche.1 ,
I assume that you followed the step from the video.
Please can you send me a screenshot of your project explorer on the left side of CubeIde and the complete log from the CubeIde Console when you hit the hammer (build button).
Regards,
Kevin
2022-01-31 9:44 AM
Yes, I followed the steps. Basically just unzipped, imported and built.
2022-02-15 9:30 AM
Hello @msche.1 ,
Sorry for the late reply.
I was finally able to work on your problem by installing the VM and trying to build.
I encountered the same issue than you by using the content described in the video.
The video was made with ecosystem 1.0.0 which is very old and with the tool STM32Workbench, which is now replaced by STM32CubeIDE, so the project syntax was different. That is why you were enable to build the project.
Procedure:
https://drive.google.com/drive/u/0/folders/1KQGGmHOE9Zq44O6KfNqAYMaGgkYwt42h
and download the folder "WorkshopUpdates_3_0_0-1.zip", which contains all the projects updated for the latest OSTL version.
Click on finish and select "DK2_TIMER1_OpenAmp_Solution_CM4" in the project explorer and click on the build icon (hammer):
You must be able to build the project.
If you want to do the other video, please keep in mind that the slides in the "WorkshopSlides" folder are the one up to date.
Hope it helps,
Regards,
Kévin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-02-23 3:08 AM
Hello @msche.1 ,
Did it fix your issue?
Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'