2022-07-19 11:39 PM
the ssh print:
U-Boot 2021.10-stm32mp-r1 (Jul 20 2022 - 10:52:56 +0800)
CPU: STM32MP157DAA Rev.Z
Model: STMicroelectronics STM32MP157D eval daughter
Board: stm32mp1 in trusted - stm32image mode (st,stm32mp157d-ed1)
DRAM: 1 GiB
Clocks:
- MPU : 650 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
WDT: Started with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0, STM32 SD/MMC: 1
Loading Environment from nowhere... OK
In: serial
Out: serial
Err: serial
invalid MAC address 0 in OTP 00:00:00:00:00:00
Net:
Error: ethernet@5800a000 address not set.
No ethernet found.
Hit any key to stop autoboot: 0
Boot over usb0!
DFU alt info setting: done
crq->brequest:0x0
#
and no more.
2022-07-20 01:02 AM
Hi @zxiao.4 ,
could you try first cleanup your SD-Card by using FlashLayout_eval_stm32mp157d-ev1-deleteall.tsv provided in Starter package ?
Regards,
2022-07-20 01:10 AM
Hi,
Please precise which board your are using (ST board or custom board) and if you use Starter Package or custom built package.
Seems you are using a starter PAckage ed1 image (intended for STM32MP157D-EV1 board, daughter board alone), but sound strange that MPU is 650MHz and not 800MHz and MAC address is not already set in OTP.
Is this board was working with Ecosystem v3.1 Starter Package ?
Regards.
2022-07-20 01:48 AM
I used custom board.Maybe I mixed them up. I'll try again
2022-07-20 02:07 AM
I don't know why this phenomenon occurs. I have changed the device tree of TF-A and u-boot from stm157d-ed1. My MPU should work at 800MHz.