Hi:
I'm using st-image-weston-openstlinux-weston-stm32mp1.ext4. The USB mouse works, but the touch screen doesn't respond.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-01 4:36 AM
Using hexdump /dev/input/event1, you can see the data changes. when I use ts_ test command, "open fbdevice: no such file or directory" will appear. Please help me, I really don't know how to configure it.I am sure that the touch screen monitoring is correct and the data is uploaded correctly.
Solved! Go to Solution.
- Labels:
-
STM32MP15 Lines
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-11 12:12 AM
I've fixed it. It should be the problem of touch coordinates. I just rotate in the device tree and reverse direction.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-04 2:13 AM
Hi @zxiao.4​ ,
I need additional information in order to find the problem.
Can you tell me which card you use and which version of openstlinux ?
What did you do for the moment ?
Did you follow the distribution package ?
regards,
Grégory
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-04 5:48 PM
Hi:
I use a customized board, similar to stm32mp157d-dk1. Opstlinux 5.15.04 kernel. The error log of Weston is as follows:​
read-back format: BGRA
EGL Wayland extension: yes
[13:49:56.022] event0 - gpio-keys: is tagged by udev as: Keyboard
[13:49:56.022] event0 - gpio-keys: device is a keyboard
[13:49:56.050] event1 - generic ft5x06 (82): is tagged by udev as: Touchscreen
[13:49:56.056] event1 - generic ft5x06 (82): device is a touch device
[13:49:56.264] libinput: configuring device "gpio-keys".
[13:49:56.265] Touchscreen - generic ft5x06 (82) - /sys/devices/platform/soc/40013000.i2c/i2c-1/1-0038/input/input1/event1
[13:49:56.265] libinput: configuring device "generic ft5x06 (82)".
[13:49:56.265] input device event1 has no enabled output associated (none named), skipping calibration for now.
[13:49:56.265] DRM: head 'DPI-1' updated, connector 32 is connected, EDID make 'unknown', model 'unknown', serial 'unknown'
[13:49:56.266] DRM: head 'DPI-1' found, connector 32 is connected, EDID make 'unknown', model 'unknown', serial 'unknown'
[13:49:56.267] Registered plugin API 'weston_drm_output_api_v1' of size 12
[13:49:56.267] Color manager: no-op
[13:49:56.268] Output 'DPI-1' using color profile: built-in default sRGB SDR profile
[13:49:56.307] Chosen EGL config details: id: 11 rgba: 8 8 8 0 buf: 24 dep: 0 stcl: 0 int: 1-60 type: win|pix|pbf|swap_preserved vis_id: XRGB8888 (0x34325258)
[13:49:56.307] Output DPI-1 (crtc 37) video modes:
1024x600@60.0, preferred, current, 51.2 MHz
[13:49:56.308] associating input device event0 with output DPI-1 (none by udev)
[13:49:56.308] associating input device event1 with output DPI-1 (none by udev)
[13:49:56.310] Output 'DPI-1' enabled with head(s) DPI-1
[13:49:56.310] Compositor capabilities:
arbitrary surface rotation: yes
screen capture uses y-flip: yes
cursor planes: yes
arbitrary resolutions: no
view mask clipping: yes
explicit sync: yes
color operations: no
presentation clock: CLOCK_MONOTONIC, id 1
presentation clock resolution: 0.000000001 s
[13:49:56.315] Loading module '/usr/lib/weston/desktop-shell.so'
[13:49:56.331] launching '/usr/libexec/weston-keyboard'
[13:49:56.336] Warning: support for deprecated wl_shell interface is enabled. Please migrate legacy clients to xdg-shell.
[13:49:56.339] Loading module '/usr/lib/weston/systemd-notify.so'
[13:49:56.341] launching '/usr/libexec/weston-desktop-shell'
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-04 5:51 PM
input device event1 has no enabled output associated (none named), skipping calibration for now.
​
I think this should be the reason for the mistake, but I don't know how to correct it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-05 5:37 AM
Hello,
Could you share me your device tree In order to check if the I2C is well configured.
regards,
Grégory
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-05 4:35 PM
&i2c2 {
ft5x06: ft5x06@38 {
compatible = "edt,edt-ft5x06","edt,edt-ft5406";
interrupt-parent = <&gpioi>;
interrupts = <1 IRQ_TYPE_EDGE_FALLING>; /* TOUCH_INT# */
vcc-supply = <&v3v3>;
reg = <0x38>;
reset-gpios = <&gpioh 15 GPIO_ACTIVE_LOW>; /* TOUCH_RESET# */
touchscreen-size-x = <1024>;
touchscreen-size-y = <600>;
status = "okay";
};
};
​
root@stm32mp1:~# evtest
No device specified, trying to scan all of /dev/input/event*
Available devices:
/dev/input/event0: gpio-keys
/dev/input/event1: generic ft5x06 (82)
Select the device event number [0-1]: 1
Input driver version is 1.0.1
Input device ID: bus 0x18 vendor 0x0 product 0x0 version 0x0
Input device name: "generic ft5x06 (82)"
Supported events:
Event type 0 (EV_SYN)
Event type 1 (EV_KEY)
Event code 330 (BTN_TOUCH)
Event type 3 (EV_ABS)
Event code 0 (ABS_X)
Value 574
Min 0
Max 1023
Event code 1 (ABS_Y)
Value 70
Min 0
Max 599
Event code 47 (ABS_MT_SLOT)
Value 0
Min 0
Max 4
Event code 53 (ABS_MT_POSITION_X)
Value 0
Min 0
Max 1023
Event code 54 (ABS_MT_POSITION_Y)
Value 0
Min 0
Max 599
Event code 57 (ABS_MT_TRACKING_ID)
Value 0
Min 0
Max 65535
Properties:
Property type 1 (INPUT_PROP_DIRECT)
Testing ... (interrupt to exit)
Event: time 1659402314.202796, type 3 (EV_ABS), code 57 (ABS_MT_TRACKING_ID), value 6
Event: time 1659402314.202796, type 3 (EV_ABS), code 53 (ABS_MT_POSITION_X), value 348
Event: time 1659402314.202796, type 3 (EV_ABS), code 54 (ABS_MT_POSITION_Y), value 416
Event: time 1659402314.202796, type 1 (EV_KEY), code 330 (BTN_TOUCH), value 1
Event: time 1659402314.202796, type 3 (EV_ABS), code 0 (ABS_X), value 348
Event: time 1659402314.202796, type 3 (EV_ABS), code 1 (ABS_Y), value 416
Event: time 1659402314.202796, -------------- SYN_REPORT ------------
Event: time 1659402314.214664, type 3 (EV_ABS), code 53 (ABS_MT_POSITION_X), value 347
Event: time 1659402314.214664, type 3 (EV_ABS), code 0 (ABS_X), value 347
Event: time 1659402314.214664, -------------- SYN_REPORT ------------
Event: time 1659402314.296616, type 3 (EV_ABS), code 57 (ABS_MT_TRACKING_ID), value -1
Event: time 1659402314.296616, type 1 (EV_KEY), code 330 (BTN_TOUCH), value 0
Event: time 1659402314.296616, -------------- SYN_REPORT ------------
​
I can detect events, but the screen just doesn't respond.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-09 2:17 AM
Hello,
I am looking for the cause of the problem and I need to know your use case to try to understand.
Regards,
Grégory
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-08-11 12:12 AM
I've fixed it. It should be the problem of touch coordinates. I just rotate in the device tree and reverse direction.