2022-01-21 11:12 AM
“Error: failed to download Segment[0]�?
I looked at the other items with the same title but did not see an answer that would help me.
I am using the STM32MP157F-DK2
The demo code was working when box was opened
I tried to run the demo
“Populate the target and boot the image�?
at
https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2
I am using ecosystem release v3.1.0
And
STM32CubeProgrammer 2.9.0
Down load eventually fails with “Error: failed to download Segment[0]�?
Any help on the matter would be appreciated
Below is the Log
10:53:37 : USB speed : High Speed (480MBit/s)
10:53:37 : Manuf. ID : STMicroelectronics
10:53:37 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
10:53:37 : SN : 002A001B3438511436383238
10:53:37 : FW version : 0x0110
10:53:37 : Board : --
10:53:37 : Device ID : 0x0500
10:53:48 : Start Embedded Flashing service
10:53:48 : Memory Programming ...
10:53:48 : Opening and parsing file: tf-a-stm32mp157f-dk2-usb.stm32
10:53:48 : File : tf-a-stm32mp157f-dk2-usb.stm32
10:53:48 : Size : 225596 Bytes
10:53:48 : Partition ID : 0x01
10:53:48 : Download in Progress:
10:53:48 : File download complete
10:53:48 : Time elapsed during download operation: 00:00:00.473
10:53:48 : RUNNING Program ...
10:53:48 : PartID: :0x01
10:53:48 : Start operation done successfully at partition 0x01
10:53:48 : Flashlayout Programming ...
10:53:48 : Running Flashlayout Partition ...
10:53:48 : Flashlayout partition started successfully
10:53:48 : Memory Programming ...
10:53:48 : Opening and parsing file: fip-stm32mp157f-dk2-trusted.bin
10:53:48 : File : fip-stm32mp157f-dk2-trusted.bin
10:53:48 : Size : 1090807 Bytes
10:53:48 : Partition ID : 0x03
10:53:48 : Download in Progress:
10:53:50 : File download complete
10:53:50 : Time elapsed during download operation: 00:00:01.428
10:53:50 : RUNNING Program ...
10:53:50 : PartID: :0x03
10:53:50 : Reconnecting the device ...
10:53:53 : USB speed : High Speed (480MBit/s)
10:53:53 : Manuf. ID : STMicroelectronics
10:53:53 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
10:53:53 : SN : 002A001B3438511436383238
10:53:53 : FW version : 0x0110
10:53:53 : Board : --
10:53:53 : Device ID : 0x0500
10:53:53 : Device name : STM32MP157FAC Rev.Z
10:53:53 : Device type :
10:53:53 : Device CPU :
10:53:53 : Start operation done successfully at partition 0x03
10:53:53 : Memory Programming ...
10:53:53 : Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32
10:53:53 : File : tf-a-stm32mp157f-dk2-sdcard.stm32
10:53:53 : Size : 225489 Bytes
10:53:53 : Partition ID : 0x04
10:53:53 : Download in Progress:
10:53:56 : Error: failed to download Segment[0]
10:53:56 : Error: failed to download the File
10:53:56 : Error: Download partition 0x04 failed
10:53:56 : Error: TSV flashing service failed
10:53:56 : Warning: Connection to device 0x500 is lost
10:53:56 : Disconnected from device.
Solved! Go to Solution.
2022-02-03 2:04 AM
Hello @JAmia.1 ,
We identified an issue with 1 or 2 faulty boards, out of the box, with the same symptoms than yours, when running at 800MHz.
Unfortunately, you have to contact your supplier to have your board replaced.
Or you can continue to use it, but with 157c-dk2 files only.
Regards,
Kevin
2022-01-28 3:40 AM
Hello @JAmia.1 ,
Do you still need help on this error?
Regards,
Kevin
2022-01-28 10:39 AM
Yes. I discovered that the failure point is random, I upgraded ubuntu to 20.4 with no change reloaded ad re decompresses the 21-11-17_tar_v3.1.0 tar. If I use the wrong file "FlashLayout_sdcard-stm32mp157d-dk1-trusted.tsv" the cube program actually works as does the stm32mp157F-dk2 once loaded with the 2016? version
as previously stated ""FlashLayout_sdcard-stm32mp157f-dk2-trusted.tsv"" randomly fails during programing sect 5 or 6 up to 11
2022-01-28 11:24 AM
I also tried to use the cube command line version on a older Linux virtual machine (I'm using A lenovo laptop ) Same failure
2022-01-28 12:19 PM
I can create a 157F-dk2 image using the example @
https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command
2022-01-28 12:40 PM
I still would like help getting the Cube Programmer working
2022-01-31 7:26 AM
Hi @JAmia.1 ,,
You said that you already tried the command line, but please can you try again to run the command line version of cube programmer 2.9.0. Run this command:
STM32_Programmer_CLI -c port=usb1 -vb 2 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157f-dk2-trusted.tsv
from your folder
STM32MP15-Ecosystem-v3.1.0/Starter-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/images/stm32mp1
And send here the complete log.
I will have a look at them.
Do you also use a virtual machine for Ubuntu?
Regards,
Kevin
2022-02-01 7:20 AM
I did exactly what you asked it just returned "STM32_Programmer_CLI: command not found"
Let me repeat my steps
1) tried running the example
“Populate the target and boot the image�?
at
https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2
I am using ecosystem release v3.1.0
And
STM32CubeProgrammer 2.9.0
on A lenovo lap top T420 first running Ubuntu 18 now upgraded to 20.4. First Entry includes the data log. Error happens at random sectors (4 or 5 some times as high as 11) (No predictable failure point rather random)
2) A co worker had an older stm32 development board working on a virtual machine using a command line and my files (aka FlashLayout_sdcard_stm32mp157f-dk2-trusted.tsv) and support files down loaded from the previous step. The results looked the same random failure point (Data log looked very similar to the above aka first entry in this thread)
3) Now we are back to my laptop. I tried to use an older file 157d-dk1- and the process worked and I could reboot the stm32 board and it worked
4) assuming that maybe something went wrong with the 157f file I re down loaded / unpacked the project. No difference
What do you want me to do next?
2022-02-01 7:32 AM
Hello @JAmia.1 ,
I understood your problem, but I used again the file from v3.1.0 ecosystem as shown in my previous post and it worked with my DK2, so it doesn't seem to be a problem related to the delivery.
Normally if you followed the page “Populate the target and boot the image�?, you should have added the path of CubeProgrammer into your path:
Add the STM32CubeProgrammer binary path to your PATH environment variable:
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH
In your case you must replace x.y.z by 2.9.0.
This binary STM32_Programmer_CLI is available in your STM32CubeProgrammer folder:
/home/osboxes/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-2.9.0/bin/STM32_Programmer_CLI
As explained in: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start/Populate_the_target_and_boot_the_image#Overview
So please, can you modify your path as explained here and try again the command that I sent before.
The goal is to have the traces of the download to see what is your issue.
Regards,
Kevin
2022-02-01 12:49 PM
I got the following
//****************************************************************************
-------------------------------------------------------------------
STM32CubeProgrammer v2.9.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
SN : 002A001B3438511436383238
FW version : 0x0110
Board : --
Device ID : 0x0500
AREA NAME SECT.NBR PARTITION.ID SIZE TYPE
fsbl1 0000 0x00000004 0256 KB RW
fsbl2 0000 0x00000005 0256 KB RW
fip 0000 0x00000006 0004 MB RW
boot 0000 0x00000010 0064 MB RW
vendorfs 0000 0x00000011 0016 MB RW
rootfs 0000 0x00000012 0744 MB RW
userfs 0000 0x00000013 14364 MB RW
virtual 0000 0x000000f1 0512 B RW
OTP 0000 0x000000f2 1024 B RW
PMIC 0000 0x000000f4 0008 B RW
Device name : STM32MP157FAC Rev.Z
Device type : MPU
Revision ID : --
Device CPU : Cortex-A7
Start Embedded Flashing service
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
Flashing service completed successfully
//*******************************************************************************************
It happened instantaneously (there is no way it actually programmed the SD card)
is this what you were looking for?