cancel
Showing results for 
Search instead for 
Did you mean: 

Don't detects the board IP address. (Getting started STM32MP157x-DK2)

Miii
Associate

I'm trying develop on Cortex-M4 of "Getting started STM32MP157x-DK2".

I have a problem that don't detects the board IP address when "6 Check connection to the target" of Modify, rebuild and reload firmware.

However, Linux prompt are displayed in the console windows by clicking on the "STM32 butterfly button" and I can run Linux command on the board.

Serial target widget status icon is yellow light, and status is "idle".

I read STM32CubeIDE support wiki page (this page), but I can't discover solution this problem.

Are there any other settings that should be made?

Am I missing something?

I use STM32CubeIDE on Windows10 OS.

I'm not familiar English, so I'm sorry if my sentence is strange.

Best regards.

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @真çÂ�?†å­Â�? 石井​ ,

How did you connect your board to ethernet .?

With ethernet cable through a LAN ?

With ethernet over USB using DK2 CN7 ?

What gives "ifconfig" command on the target ?

Are you able to ping the board ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.