2021-12-21 11:21 AM
IDE suggested that I upgrade STLink FW on my STM32MP1-DK2 discovery board. Now when I connect my Linux PC to USBC on DK2, device isn't recognized by STMProgrammer (also nothing shows up in dmesg).
Solved! Go to Solution.
2021-12-21 11:38 PM
Hi @BBeck.1 ,
There's no relation between ST-Link and USBC on DK2.
It's 2 different physical ports on board and drivers on PC side.
When you say IDE ? You mean STM32CubeIDE ?
>> USBC on DK2, device isn't recognized by STMProgrammer
Using CubeProg GUI ? Do you select USB as device for connection ?
Do you set boot switch to 00 for serial boot ?
Could you send a screenshot ?
>> also nothing shows up in dmesg
This case you mean with SDCard boot.
Nothing display on ST-Link Virtual Com Port console, right ?
But does the boot looks to happen with demo launcher displayed on sreen ?
Thanks
Olivier
2021-12-21 11:38 PM
Hi @BBeck.1 ,
There's no relation between ST-Link and USBC on DK2.
It's 2 different physical ports on board and drivers on PC side.
When you say IDE ? You mean STM32CubeIDE ?
>> USBC on DK2, device isn't recognized by STMProgrammer
Using CubeProg GUI ? Do you select USB as device for connection ?
Do you set boot switch to 00 for serial boot ?
Could you send a screenshot ?
>> also nothing shows up in dmesg
This case you mean with SDCard boot.
Nothing display on ST-Link Virtual Com Port console, right ?
But does the boot looks to happen with demo launcher displayed on sreen ?
Thanks
Olivier
2021-12-22 7:43 AM
Thanks. Yeah, I hadn't plugged in the OTHER usbc port (which is the DFU) on the DK2 board. Anyhow, it was coincidental that The Cube IDE prompted for ST-link upgrade.
I appreciate your response.
Cheers,
Ben
2021-12-22 7:46 AM
Hi @BBeck.1
Thanks for feedback !
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'