2021-08-01 11:27 PM
2021-08-03 06:27 AM
However if you can move to openstlinux v3.0 it will likely solve your issue.
2021-08-03 06:49 AM
Will try that
2021-08-03 11:34 PM
we are working on a sip based on stm32mp157c ,we are using a sdk for building the kernel for a developer package the sdk only supports v2.0
is there an sdk that supports v3.0??
2021-08-04 08:59 AM
2021-08-04 07:59 PM
the problem.was with the internet connectivity fixed it and installed devmem2 now its working fine
Thank you for your help
2021-08-04 10:00 PM
Hi OliverK
Is there a way to establish communication with the coprocessor in the stm32mp157c
2021-08-05 05:28 AM
Hi KS.2 (Community Member)
Please close this topic and open a new one for clarity.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
For the coprocessor topic this is where to start:
https://wiki.st.com/stm32mpu/wiki/Coprocessor_management_overview