cancel
Showing results for 
Search instead for 
Did you mean: 

DDR Bus Test Error in STM32MP157AAD3 before FSBL, How to resolve this?

BG.3
Associate III

Our board is similar to STM32MP157C-DK2 Disco board - All the Developer packages have been installed, When the power supply is given, all the test point voltages are in desired level. But the MPU not even clearing FSBL and exit with

ERROR: DDR addr bus test: can't access memory @ 0xc0000004

PANIC at PC : 0x2ffdf9d9

Exception mode=0x00000016 at: 0x2ffda000

What is the issue and how we can address?

10 REPLIES 10
PatrickF
ST Employee

Hi,

There is many FAQ which could help:

from this page : https://community.st.com/s/article/FAQ-STM32MP1-Bring-up-procedure you could find many links/information.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thank you so much for responding. I'll look into it.

DG
Associate II

Hello, have you solved the problem? I have encountered a similar problem.

BG.3
Associate III

No, Still the issue remains.

Hello, Nothing new, I have the same problem too

i have the same problem i did not get the correct output 

Hi i am facing the same issue please help me out this ,
i am waiting for your response @PatrickF 

PatrickF
ST Employee

Hi,

error message is usually just not enough to help.

We need more information on your setup (HW, SW, board, etc...) and the check you already done (supplies, soldering, etc...).
For DDR, even if slightly outdated, this page could help to go further

https://community.st.com/t5/stm32-mpus/faq-stm32mp1-how-to-validate-the-stm32mp1-dram-connection-on-pcb/ta-p/49270

Community is not a simple question/answer tool, but a sharing platform intended to raise knowledge and allows people to find themself the solution or the path for deeper investigation.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

I think the ISSUE with the PMIC it won't supply the voltage to the ddr.
I Read the datasheet of PMIC i Found that my DDR is connected to PMIC buck 2 which is RANK 0.
i do not know anything of that. 
who are RANK 0 in PMIC are not supplied the power.
so where i need to modify and TF-A then it work.