2022-04-09 12:49 AM
Our board is similar to STM32MP157C-DK2 Disco board - All the Developer packages have been installed, When the power supply is given, all the test point voltages are in desired level. But the MPU not even clearing FSBL and exit with
ERROR: DDR addr bus test: can't access memory @ 0xc0000004
PANIC at PC : 0x2ffdf9d9
Exception mode=0x00000016 at: 0x2ffda000
What is the issue and how we can address?
2022-04-11 12:10 AM
Hi,
There is many FAQ which could help:
from this page : https://community.st.com/s/article/FAQ-STM32MP1-Bring-up-procedure you could find many links/information.
Regards.
2022-04-11 9:08 AM
Thank you so much for responding. I'll look into it.
2023-03-19 5:52 PM
Hello, have you solved the problem? I have encountered a similar problem.
2023-03-22 12:11 AM
No, Still the issue remains.
2024-01-22 2:00 AM
Hello, Nothing new, I have the same problem too
2024-09-05 5:00 AM
i have the same problem i did not get the correct output
2024-09-05 5:02 AM
Hi i am facing the same issue please help me out this ,
i am waiting for your response @PatrickF
2024-09-05 5:21 AM
Hi,
error message is usually just not enough to help.
We need more information on your setup (HW, SW, board, etc...) and the check you already done (supplies, soldering, etc...).
For DDR, even if slightly outdated, this page could help to go further
Community is not a simple question/answer tool, but a sharing platform intended to raise knowledge and allows people to find themself the solution or the path for deeper investigation.
Regards.
2024-09-06 4:33 AM
I think the ISSUE with the PMIC it won't supply the voltage to the ddr.
I Read the datasheet of PMIC i Found that my DDR is connected to PMIC buck 2 which is RANK 0.
i do not know anything of that.
who are RANK 0 in PMIC are not supplied the power.
so where i need to modify and TF-A then it work.