cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot run DDR test suite on STM32MP157D-DK1

--.2
Associate

Hello, I want to use DDR test suite in STM32 cube IDE but I always have a error when I try to connect my board. I think I understood that was because I have to modify something with stage boot with SPL. I red the docs but I am quite lost can someone give me the steps to make DDR test suite work ?

Kind regards

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @--.2​ ,

Yes indeed DDR Tuning tool require to build and load U-Boot SPL

Please read here :

U-Boot SPL: DDR interactive mode - stm32mpu

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.