2024-07-14 03:42 PM
Dear Team,
I have got the a STM32MP257F-EV1 ( MB 1936A ) board.
I tried the following steps to build the YOCTO image( after pulling the source ).
DISTRO=openstlinux-weston MACHINE=stm32mp2 source layers/meta-st/scripts/envsetup.sh
bitbake st-image-weston
The build was successful, but after the build finished, I was able to see the multiple .tsv files.
I selected "FlashLayout_sdcard_stm32mp257f-ev1-fastboot.tsv" to create the SD card image.
I used the script "create_sdcard_from_flashlayout.sh" to create the raw image. I flashed the raw image in the sd card and placed the card in the board. Boot dip switch setting was 0 0 0 1 (0th bit was on). After powering on I can see all the LEDs are ok. but there is no message over the console. Hence concluded the board is not booting. and always getting detected as DFU board. even after changing the boot switch.
Please suggest how can I fix this issue.
Thank you.
Regards,
Zafar