cancel
Showing results for 
Search instead for 
Did you mean: 

I can not download android starter image to stm32MP1-DK 2 board.

Sergey1
Associate III

I am using starter image "en.st-android-10.0.0-2020-02-21-eval-sd-starter.tar.gz".

CubeProgrammer gave me "Error: an error occurred while uploading data from the virtual partition 0xF1" . Below is full log:

16:56:19 : USB speed : High Speed (480MBit/s)

16:56:19 : Manuf. ID : STMicroelectronics

16:56:19 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

16:56:19 : SN : 0046003E3338510634383330

16:56:19 : FW version : 0x0110

16:56:19 : Device ID : 0x0500

16:56:23 : Start Embedded Flashing service

16:56:23 : Memory Programming ...

16:56:23 : Opening and parsing file: fsbl-programmer.img

16:56:23 : File : fsbl-programmer.img

16:56:23 : Size : 245360 Bytes

16:56:23 : Partition ID : 0x01 

16:56:23 : Download in Progress:

16:56:24 : File download complete

16:56:24 : Time elapsed during download operation: 00:00:00.431

16:56:24 : RUNNING Program ... 

16:56:24 : PartID: :0x01 

16:58:14 : Error: an error occured while uploading data from the virtual partition 0xF1

16:58:14 : Start operation done successfully at partition 0x01

12 REPLIES 12

Hello Mr. @Nicolas L​ 

thank you so much for your instructions,

may you help me solve this issue please, when you have time.

[ 6% 4099/66511] build fsbl.img

FAILED: fsbl.img

/bin/bash -c "(prebuilts/build-tools/linux-x86/bin/acp -fp device/stm/stm32mp1-bootloader/prebuilt/fsbl/tf-a-stm32mp157c-dk2-trusted.stm32 out/target/product/disco/fsbl-trusted.img ) && (prebuilts/build-tools/linux-x86/bin/acp -fp device/stm/stm32mp1-bootloader/prebuilt/fsbl/tf-a-stm32mp157c-dk2-optee.stm32 out/target/product/disco/fsbl-optee.img ) && (prebuilts/build-tools/linux-x86/bin/acp -fp device/stm/stm32mp1-bootloader/prebuilt/fsbl/tf-a-stm32mp157c-dk2-programmer.stm32 out/target/product/disco/fsbl-programmer.img )"

acp: file 'device/stm/stm32mp1-bootloader/prebuilt/fsbl/tf-a-stm32mp157c-dk2-programmer.stm32' does not exist

[ 6% 4101/66511] Build hyb out/target/product/disco/obj/ETC/hyph-nn_intermediates/hyph-nn.hyb <- external/hyphenation-patterns/nn//hyph-nn.pat.txt

12585 unique nodes, 42861 total

[ 6% 4102/66511] Build hyb out/target/product/disco/obj/ETC/hyph-nb_intermediates/hyph-nb.hyb <- external/hyphenation-patterns/nb//hyph-nb.pat.txt

12585 unique nodes, 42861 total

[ 6% 4104/66511] Build hyb out/target/product/disco/obj/ETC/hyph-hu_intermediates/hyph-hu.hyb <- external/hyphenation-patterns/hu//hyph-hu.pat.txt

21515 unique nodes, 102669 total

11:27:48 ninja failed with: exit status 1

#### failed to build some targets (02:41 (mm:ss)) ####

PZwei.1
Associate

Hi @Nicolas L (ST Employee)​ 

It's possible to receive those sources and directives too?

Thanks a lot,

Patrick

RMako.1
Associate

The other option to fix Chrome can't download images on Android is to clear its data and cache. Doing so will reset the browser to default settings. However, it will not delete your downloaded data. Open Settings on your phone.