2022-03-06 3:39 AM - last edited on 2023-07-13 8:24 AM by Kevin HUBER
Hello,
I am working on a custom Boot Loader (SSBL) for the STM32MP157F-EV1 board to replace U-Boot in the boot chain (BL33), this is a requirement for my project.
As I understand, to boot the Linux Kernel it is needed to provide 3 values through the first 3 registers as follows:
What would be the MACH_TYPE needed to pass to the linux kernel to boot through the register R1?
The list of MACH_TYPES can be found in https://elixir.bootlin.com/linux/v5.17-rc6/source/arch/arm/tools/mach-types. But I do not find an specific one for this board or any stm MPU.
Thank you,
Andrés Gamboa
2022-05-18 11:36 PM
Hello Gamboa
For a DT-only BSP the MACH_TYPE should be all 1 (~0) as explained in below article
https://elixir.bootlin.com/linux/v5.15.41/source/Documentation/arm/booting.rst#L78
For DT-only platforms, the machine type will be determined by device
tree. set the machine type to all ones (~0). This is not strictly
necessary, but assures that it will not match any existing types.
JM