2020-09-10 7:15 PM - last edited on 2023-07-13 8:14 AM by Kevin HUBER
Hi
The terminal printing information is as follows.
This TF-A will start properly in EMMC.
In the docs/plat/stm32mp1.rst file, I saw that USB is not supported. May I ask how to modify it so that it can be burned via USB
Regards
User.44
Solved! Go to Solution.
2020-09-14 6:13 AM
Here is the new file you can replace "Makefile.sdk" from the V2.0.0/.../tf-a-stm32mp-2.2.r1-r0/ directory (obviously, you need to remove .txt extension).
2020-09-11 1:23 AM
Hi @文�?� �?
This is a known issue we have recently discovered internally also.
I come back to you shortly.
Olivier
2020-09-14 5:17 AM
In the developer package, the Makefile.sdk for tf-a was not well generated and it needs revision for the "serialboot" build.
A new Makefile.sdk will be delivered in this post that will solve this issue.
2020-09-14 5:32 AM
Hi Bernard PUEL
The article
2020-09-14 6:13 AM
2020-09-14 6:33 AM
Hi Bernard PUEL
Thank you very much for bothering me for 3 days