2021-02-01 2:54 AM
I'm trying to use PA10 to drive a simple LED (custom board), but the I/O doesn't switch at all.
PA10 is not used in any of the device trees.
gpioinfo gpiochip0
reports the I/O as "unused" and "output", but switching the I/O with
gpioset gpiochip0 10=1
doesn't work. The voltage on the pin stays at 1.7V.
PA10 can also function as OTG_FS_ID or OTG_HS_ID, so maybe this causes problems? I do not use USB in my kernel device tree.
2021-02-01 4:55 AM
Please check uBoot DT regarding PA10, which might still be activated as OTG_ID pin.
See https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board#USB_OTG_node
Regards.
2021-02-01 6:10 AM
My u-boot devicetree contains:
&usbotg_hs{
u-boot,dm-pre-reloc;
/* USER CODE BEGIN usbotg_hs */
u-boot,force-b-session-valid;
hnp-srp-disable;
dr_mode = "peripheral";
/* USER CODE END usbotg_hs */
};
So, the ID pin should be unused in uBoot?
2021-02-01 6:19 AM
Are you using the latest Openstlinux-5.4-dunfell-mp1-20-11-12 ?
2021-02-01 6:47 AM
I'm at 20-06-24 with DISTRO_VERSION 3.1-snapshot-20210201
2021-02-08 7:51 AM
Hi allard (Community Member),
VDD3V3_USBFS is used to supply OTG_VBUS and OTG_ID (PA10) pins. So,
VDD3V3_USBFS must be supplied as well when USB high-speed dual-role-port or USB
high-speed device is used. If not used, should be connected to VDD.
This is an extract of the App note
Regards,
Olivier