2019-11-14 01:35 AM - last edited on 2023-07-13 07:59 AM by Kevin HUBER
Hi, I need to save a variable from u-boot console but is not possible because the command SAVEENV is disabled (STM32MP1 module) .
How can I do?
2019-12-04 08:13 AM
Maybe you are not on the latest delivery version because saveenv is working on V1.1.0 release (openstlinux-4.19-thud-mp1-19-10-09 tag).
STM32MP> saveenv
Saving Environment to EXT4... Recovery required
file found, deleting
update journal finished
File System is consistent
update journal finished
done
OK
STM32MP>
The feature was enabled starting with u-boot tag: v2018.11-stm32mp-r3