How to Know the reset reason in uboot instead of Primary Bootloader
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-05-13 12:24 AM
Hi,
I have an STM32MP157C-DK2 reference board and it is booting with yocto linux.From the bootlog I came to know that reset reason is checked in the Primary Bootloader by reading a register from the file tf-a-stm32mp/plat/st/stm32mp1/bl2_plat_setup.c
uint32_t rstsr = mmio_read_32(stm32mp_rcc_base() + RCC_MP_RSTSCLRR);
Now I want to know the reason in the uboot level before lauching the kenel image to add an extra environmental variable in uboot.I tried to read the register using readl(),_raw_readl() API's but I was throwing data abort error while booting and the board gets reboot.So I need help w.r.t the way to read register or any other way to get the reset reason information.
Regards
Srikanth.
- Labels:
-
OpenSTLinux
-
ST-Boards
-
STM32MP15 Lines
-
Yocto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-12 10:13 AM
The RCC_MP_RSTSCLRR is always readable even in nonsecure mode, you should be able to read it.
I suggest to use asm("bkpt") in uboot at place where you want to read it, use openocd to check
the register (and maybe MMU tables - mdw phys is your friend).
Other way is to copy the value into some of TEMP registers in TF-A and read back in u-boot. TEMPs
are already used for similar things.
regards, Martin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-29 7:00 AM
Hi,
in Table 74. Register access type versus protection and security (continued)
RCC_MP_RSTSCLRR, RCC_MP_RSTSSETR
Access types = SR/CR
Access limitations = N
Secure attribute = S
Secure control bits = TZEN
=> only secure can write to this register / controlled by TZEN but read is allowed
After check with memory dump command (md), in U-Boot read is allowed :
STM32MP> md 50000408 1
50000408: 00000014
regard
Patrick