2024-08-19 3:45 AM - edited 2024-08-22 3:47 AM
Hello @Erwan SZYMANSKI
I hope your week started well.
I think the script didn’t work because I couldn't adjust the paths correctly. Could you please assist me in finding the correct paths and adjusting my script accordingly?
# !/bin/sh
export QSG_INFO=1
export QML2_IMPORT_PATH=~/imports/
export PATH=/usr/local/qt5-install/bin/:/usr/local/apitrace/bin:$PATH
export QT_QPA_PLATFORM=wayland
#Execute the Qt program
export XDG_RUNTIME_SESSION=wayland; export XDG_RUNTIME_DIR=/run/user/1000; export WAYLAND_DISPLAY=wayland-1; cd /usr/bin && ./automotive
nesnes@nesnes-ABRA-A5-V19-2:/usr/local$ tree -L 2
.
├── bin
├── etc
├── games
├── include
├── lib
│ └── python3.10
├── man -> share/man
├── sbin
├── share
│ ├── ca-certificates
│ ├── fonts
│ ├── man
│ ├── sgml
│ ├── texmf
│ └── xml
└── src
2024-10-04 1:13 AM
@PPAGE.13I have my recipe ready. My problem is getting this error. Can you help me solve this problem. I share any file you want if you write them.
QQmlApplicationEngine failed to load component
qrc:/Wearable/Main.qml: No such file or directory
SUMMARY = "Wearable Application (Prebuilt and Compiled from Source)"
DESCRIPTION = "Includes prebuilt wearable binary and also compiles wearable2 from source"
LICENSE = "MIT"
LIC_FILES_CHKSUM = "file://${COMMON_LICENSE_DIR}/MIT;md5=0835ade698e0bcf8506ecda2f7b4f302"
# Ekstra dosya yollarını tanımlama - Yeni sözdizimi
FILESEXTRAPATHS:prepend := "${THISDIR}/files/src:"
SRC_URI = "file://src \
file://src/Wearable \
file://src/wearable.qrc"
S = "${WORKDIR}/src"
DEPENDS = "qtbase qtquickcontrols2 qtdeclarative "
inherit qmake5
# Install prebuilt wearable and build wearable2 from source
do_install() {
install -d ${D}${bindir}
install -d ${D}${datadir}/wearable
# Install prebuilt executable
install -m 0755 ${WORKDIR}/src/wearable ${D}${bindir}/wearable
# Build from source
cd ${S}
qmake wearable.pro # Specify the .pro file for qmake
make
# Install the source-built executable as wearable2
install -m 0755 wearable ${D}${bindir}/wearable2
# Install QML and resource files
cp -r ${WORKDIR}/src/Wearable ${D}${datadir}/wearable/
}
FILES_${PN} = "${bindir}/wearable ${bindir}/wearable2"
2024-10-04 1:25 AM
I don't see the RDEPENDS section, did you add it?
RDEPENDS¶
Lists a package's runtime dependencies (i.e. other packages) that must be installed in order for the built package to run correctly. If a package in this list cannot be found during the build, you will get a build error.
Philippe.
2024-10-04 1:32 AM
@PPAGE.13 I have rearranged my recipe , I need to flash the image to the board and that takes some time , I will reply again soon.
SUMMARY = "Wearable Application (Prebuilt and Compiled from Source)"
DESCRIPTION = "Includes prebuilt wearable binary and also compiles wearable2 from source"
LICENSE = "MIT"
LIC_FILES_CHKSUM = "file://${COMMON_LICENSE_DIR}/MIT;md5=0835ade698e0bcf8506ecda2f7b4f302"
# Extra file paths definition - Updated syntax
FILESEXTRAPATHS:prepend := "${THISDIR}/files/src:"
SRC_URI = "file://src \
file://src/Wearable \
file://src/wearable.qrc"
S = "${WORKDIR}/src"
DEPENDS = "qtbase qtquickcontrols2 qtdeclarative "
# Runtime dependencies: Ensure these are installed at runtime
RDEPENDS_${PN} = "qtbase qtquickcontrols2 qtdeclarative qtwayland qtgraphicaleffects qtquickcontrols qtquickcontrols2"
inherit qmake5
# Install prebuilt wearable and build wearable2 from source
do_install() {
install -d ${D}${bindir}
install -d ${D}${datadir}/wearable
# Install prebuilt executable
install -m 0755 ${WORKDIR}/src/wearable ${D}${bindir}/wearable
# Build from source
cd ${S}
qmake wearable.pro # Specify the .pro file for qmake
make
# Install the source-built executable as wearable2
install -m 0755 wearable ${D}${bindir}/wearable2
# Install QML and resource files
cp -r ${WORKDIR}/src/Wearable ${D}${datadir}/wearable/
cp -r ${WORKDIR}/src/WearableSettings ${D}${datadir}/wearable/
cp -r ${WORKDIR}/src/WearableStyle ${D}${datadir}/wearable/
}
FILES_${PN} = "${bindir}/wearable ${bindir}/wearable2"
2024-10-04 2:41 AM
@PPAGE.13 Still get the same error
root@stm32mp15-disco:~# wearable
QStandardPaths: runtime directory '/run/user/1000' is not owned by UID 0, but a directory permissions 0700 owned by UID 1000 GID 1000
QQmlApplicationEngine failed to load component
qrc:/Wearable/Main.qml: No such file or directory
2024-10-07 5:21 AM
Don't you have a case issue with Wearable directory, but installed in wearable?
If not, I don't have much more idea.
Philippe.