2024-02-21 9:46 AM - edited 2024-02-21 9:47 AM
Hello, I'm trying to develop a SOM device with a STM32MP153AAB3 processor, I would like to use the 2BC CYW4373 chipset, since it's dual band wifi module. The reason why I want to use this chip is because I want to be able to use it as an Access point and STA at the same time (I want to connect to internet and deploy a webserver in a desire IP at the same time, for example 2.4GHz for AP and 5G for STA). The reason why would like a support in this topic is because I don't know if the brcmfmac driver is enough to perform in both modes at the same time. I also searched in the community to see if that is possible, I found this post in another forum: https://community.infineon.com/t5/Wi-Fi-Bluetooth-for-Linux/Issue-on-Wireless-AP-STA-mode-on-BCM43455/m-p/32968#M52 .
The problem with the last post is that I'm not sure if I can apply that to the CYW4373, because the post is about another chipset.
On the other hand, MuRata has a layer for yocto https://github.com/murata-wireless. I am working with yocto, I create a personal layer for all the things I need.
The problem I found is that the layer has support for NXP devices, so I don't know if that will work with the STM32MP153AAB3 processor.