cancel
Showing results for 
Search instead for 
Did you mean: 

Developing Qt application on STM32mp157f-DK2

pauld
Associate

Hello everyone!

I'm getting started with STM32mp157f-DK2. I was able to successfully build images using Yocto as well as buildroot (using stm32mp157c config) and port various command line applications to stm32mp157f-dk2  I'm a trying to develop/port Qt, Gtk applications for the stm32mp157f-dk2 board. Also Can someone help me with how to compile Qt / Gtk applications for stm32mp157f-dk2? Is there a good documentation/guide available for that? 

Thanks in advance!

1 REPLY 1
PPAGE.13
ST Employee

Hi Paul,

 

please have a look at our Qt expansion package:

https://wiki.st.com/stm32mpu/wiki/X-LINUX-QT_Expansion_Package

For MP1 only Distribution package is supported today with X-LINUX-QT 1.0.0. Next package with full MP1 Starter/Developer/Distribution support will happen before end of 2024.

MP2 has already full support.

 

You can also check this thread:

https://stmicro.response.lithium.com/console/agent/22293782

 

BR,

Philippe

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.