cancel
Showing results for 
Search instead for 
Did you mean: 

PHYTEC STM32MP135 LCD PANEL DTS

batuhanky
Associate III

Hello everyone,

I am using the STM32MP135 SoM from PHYTEC, and I’m creating a custom device tree source (DTS) file tailored to our carrier board. I’m having trouble controlling the backlight PWM signal. I’m unable to enable the PWM and enable signal as expected, although I can change the enable pin status if I remove the enable pin definition from the backlight node. Additionally, there is no [used] indication next to GPIOI pin 0, which I’ve configured as the panel enable GPIO. I suspect this issue may be related to the LCD node configuration.

I’ve attached my GPIO states and the DTS file for reference.

image_2024-11-05_005132081.png

image_2024-11-05_005307530.png

image_2024-11-05_005326551.png

 

3 REPLIES 3
Olivier GALLIEN
ST Employee

Hi @batuhanky 

Did you try to get support from PHYTEC ? 

Thanks

Olivier 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Perhaps indicate how it would work in the generic non-board specific sense, and if the DTS file misses specific details or is otherwise internally inconsistent. 

That would be more helpful than entirely punting and might have broader impact. 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi @Olivier GALLIEN 

Thanks for your reply, they say use overlays instead of creating new dts. When I comment out the backlight property from the panel node I can control the backlight enable and pwm pins, but when I add the backlight property I can't control anything. Here is the dts that works:

     panel_rgb: rgb-panel {
		compatible = "panel-dpi";
                label = "generic-lcd";
		enable-gpio = <&gpioi 0 GPIO_ACTIVE_HIGH>;
		//backlight = <&panel_backlight>;

		data-mapping = "bgr666";

		status = "okay";

		width-mm = <115>;
		height-mm = <80>;

		port {
			panel_in_rgb: endpoint {
				remote-endpoint = <&ltdc_ep0_out>;
			};
		};
		panel-timing {
                        clock-frequency = <9800000>;
                        hactive = <480>;
			vactive = <272>;
                        hfront-porch = <39>;
			hback-porch = <39>;
			hsync-len = <4>;
			vback-porch = <29>;
			vfront-porch = <13>;
			vsync-len = <10>;
                        hsync-active = <0>;
                        vsync-active = <0>;
                        phandle = <86>;
		};
	};

    panel_backlight: panel-backlight {
        compatible = "pwm-backlight";
        status = "okay";
        pwms = <&pwm_bl 2 50000 1>;
        enable-gpios = <&gpiob 1 GPIO_ACTIVE_HIGH>;
        power-supply = <&scmi_vdd>;
        brightness-levels = <0 2 5 7 10 12 15 17 20 22 25 28 30 33 35
                            38 40 43 45 48 51 53 56 58 61 63 66 68 71
                            73 76 79 81 84 86 89 91 94 96 99 102 104
                            107 109 112 114 117 119 122 124 127 130
                            132 135 137 140 142 145 147 150 153 155
                            158 160 163 165 168 170 173 175 178 181
                            183 186 188 191 193 196 198 201 204 206
                            209 211 214 216 219 221 224 226 229 232
                            234 237 239 242 244 247 249 252 255>;
        default-brightness-level = <50>;
    };