2024-07-24 5:53 PM - edited 2024-07-24 5:55 PM
I have tried to build my own OpenSTLinux by using the SDK and the sources, without sucess. I have been trying to compile for 2 weeks from now and I'm not very pleased over the wiki of ST32MP.
Anyway. I have to show a bug. I cannot build an OpenSTLinux Project inside STM32CubeIDE.
I first created a project for my STM32MP1 processor, then I tried to attach the SDK with the STM32CubeIDE. But it did not work well.
I have STM32CubeIDE 1.16.0 and Lubuntu 22.04 and the latest SDK.
So what I'm looking for, is some way to compile the kernel, TF-A, Optee and U-boot with STM32CubeIDE. If it's possible. Or else....it's impossible to follow the wiki of STM32MP.
How to install the Yocto Project SDK in STM32CubeIDE - stm32mpu
This is my goal: How to manage OpenSTLinux projects in STM32CubeIDE - stm32mpu
Solved! Go to Solution.
2024-07-25 1:47 PM - edited 2024-07-25 1:47 PM
I found the solution. It was an issue when you're importing a project and migrate it to the latest version. Then you're about to facing these kind of issues.
So the solution was: Create a new project and copy the parameters from the .ioc file to the new one.
But...it's still a bug inside the STM32CubeIDE.
2024-07-25 1:47 PM - edited 2024-07-25 1:47 PM
I found the solution. It was an issue when you're importing a project and migrate it to the latest version. Then you're about to facing these kind of issues.
So the solution was: Create a new project and copy the parameters from the .ioc file to the new one.
But...it's still a bug inside the STM32CubeIDE.