2019-10-23 1:32 AM
Which setting do i need?
right now i try to build u-boot as debian package with follwoing settings:
dpkg-buildpackage -a arm
At the begining of the compilation i get following error:
dpkg-architecture: warning: specified GNU system type arm-linux-gnu does not match CC system type arm-openstlinux_weston-linux-gnueabi, try setting a correct CC environment variable
Nevertheless it compiles successfully but the problem is that after the comliation the packager fails with follwoing error:
Can't exec "arm-linux-gnu-objcopy": No such file or directory at /usr/share/perl5/Debian/Debhelper/Dh_Lib.pm line 475.
As you can see it search for arm-linux-gnu-objcopy and not the one i have specifed by openst-weston-compiler!
What are the right calling parameters for dpg-buildpackage and "arm-openstlinux_weston-linux-gnueabi"-Compiler ?
Thanks
2020-06-04 8:38 AM
Hi @ajava
You probably need to initialise the cross-compilation via SDK:
---------------------------------------
* Source SDK environment:
$> source <path to SDK>/environment-setup-cortexa9hf-neon-openstlinux_weston-linux-gnueabi
* To verify if you cross-compilation environment are put in place:
$> set | grep CROSS
CROSS_COMPILE=arm-openstlinux_weston-linux-gnueabi-
Warning: the environment are valid only on the shell session where you have sourced the sdk environment.
Do not hesitate to have a look at the wiki page for the STM32MP1 Developer Package: https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package_-_SDK
Best regards
Jean-Philippe