cancel
Showing results for 
Search instead for 
Did you mean: 

What is difference between OSTL v4.0.0 and OSTL v4.1.0

GChin.1
Associate II

Hi Team,

There are two version of OSTL i.e. v4.0.0  STM32 MPU OpenSTLinux release note - v4.0.0 - stm32mpu-ecosystem-v4 and v4.1.0  STM32 MPU OpenSTLinux release note - v4.1.0 - stm32mpu-ecosystem-v4.  what is difference between them both are at 5.15.x kernel and using Kirkstone? 

Is OSTL v4.1.0/v4.1.1/v4.1.2 backward compatible with v4.0.0/v4.0.1/v4.0.2? @OlivierK 

 

Thank you.

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @GChin.1 ,

Release 4.1 is a maintenance release of the 4.0 ecosystem release using same Yocto (Kirkstone) and Kernel version (5.15) 

Differences are listed in STM32 MPU OpenSTLinux release note - v4.1.0 - stm32mpu-ecosystem-v4

Even if backward compatibility may exist, we always recommend using all components version from the same version, as validated by ST. 

Note that 4.x releases are no more supported by ST and so not recommended for new design. 

Please use the latest V6 

STM32 MPU ecosystem release note - stm32mpu

Olivier 

 

 

 

 

 

 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.