2020-05-08 09:59 AM
Not sure where to post this, just unpacked a STM32MP157C-EV1 and was following the Getting started instructions. The insctructions use USB to program a SDHC card. But, on this page:
"Connect USB Type A to Type C cable between PC and CN7/USB_OTG port of the STM32MP157x-EV1 board"
But CN7/USB_OTG is on the STM32MP157C-DK2, not the -EV1 and there is no corresponding connector (I think). Will try to program the card using ST-LINK.
Thanks!
Solved! Go to Solution.
2020-05-08 02:03 PM
Well, that was simple, there is a corresponding connector, but it's not on the CPU board, it's on the peripherals board. So to I think the following change should be made to the instructions:
From:
"Connect USB Type A to Type C cable between PC and CN7/USB_OTG port of the STM32MP157x-EV1 board"
To:
"Connect USB Type A to Micro USB Type B cable between PC and CN16/USB_OTG port of the STM32MP157x-EV1 board"
Sorry if I wasted anyone's time with this.
2020-05-08 02:03 PM
Well, that was simple, there is a corresponding connector, but it's not on the CPU board, it's on the peripherals board. So to I think the following change should be made to the instructions:
From:
"Connect USB Type A to Type C cable between PC and CN7/USB_OTG port of the STM32MP157x-EV1 board"
To:
"Connect USB Type A to Micro USB Type B cable between PC and CN16/USB_OTG port of the STM32MP157x-EV1 board"
Sorry if I wasted anyone's time with this.
2020-05-10 11:41 PM
Thanks @Community member
Indeed there was a mistake in Wiki, thanks to point it and sorry for inconvenience.
Olivier