2024-08-06 03:34 AM
Hi,
At my company, we develop debuggers and are trying to access STM32MP257F-EV1(ES) board via the DAP,
Unfortunately, we are unable to access the DAP and it seems like JTAG (DAP) access is prohibited by hardware.
The result was the same even after shorting JP3 and turning off ST-LINK.
I have the following questions:
I would appreciate any response.
Thank you.
Solved! Go to Solution.
2024-08-06 11:42 PM
Hi,
in 'development boot' (BOOT=0b0011 or 0b1100), the debug is enabled and nothing specific is needed to access thru JTAG/SWD. In development boot, the red led (LD1, close to reset button) is light.
As you are building debuggers for ST chipset, There is maybe some partnership already in place. Could you give me more details on your company and if you get the board through distributor or directly from ST (by private message if you prefer).
If it helps, here is part of the T32 initialisation I use:
SYStem.RESetOut
wait 100.ms
; Cortex-A35
sys.cpu CortexA35
; JTAG/SWD freq
system.JTAGCLOCK 2M
SYSTEM.CONFIG.DEBUGPORTTYPE SWD
SYStem.CONFIG SWDP ON
; DAP Config
sys.config CHIPIRPRE 4.
sys.config CHIPDRPRE 1.
sys.config DAPIRPOST 5.
sys.config DAPDRPOST 1.
; Dual core (A35)
system.CONFIG.CoreNumber 2.
;Assign the two CA35 to this debug session
core.assign 1. 2.
; Debug base address for each core
SYStem.CONFIG.COREDEBUG.Base DAP:0x80210000 DAP:0x80310000
; Config access ports
SYStem.CONFIG MEMORYACCESSPORT 0.
SYStem.CONFIG AHBACCESSPORT 0.
SYStem.CONFIG APBACCESSPORT 0.
SYStem.CONFIG DEBUGACCESSPORT 0.
SYStem.CONFIG AXIACCESSPORT 4.
sys.o.WaitReset 1.s
sys.o.EnReset OFF
sys.o.ResBreak OFF
; connect DAP only
SYStem.Mode.Prepare
; Disable vector catch
tronchip.reset
tronchip.set reset off
tronchip.set StepVector off
; Attach and halt
sys.mode.up
if run()
break.
I you cannot progress, maybe ask for direct support to your local ST representative.
Regards.
2024-08-06 05:00 AM
Hi @Aiyps
please see some answers:
1. JP3 is not needed to allows 3rd party debugger access thru CN22. You could keep JP3 off to use STLINK VCP for console(s) even with CN22 usage
2. There is no debug authentication, but debug is not enabled in all cases. 'Development boot' could be used to debug (or need to have a SW running which enable the debug inside BSEC)
3. Unlike STM32MCUs, CubeProgrammer cannot be used with STLINK. Only USB or UART is available for download binaries. STLINK is only for debugging purpose (e.g. CubeIDE) and to show UART VCP for serial console(s)
CubeProgrammer should work to download Starter Package into flash (with adequate BOOT pins). See https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-EV1/Let%27s_start/Populate_the_target_and_boot_the_image
I personally use a 3rd party debugger (Lauterbach Trace32 PowerDebug) on EV board without issues.
Could you please precise which board revision (MB1936x) and which device revision (B, X or Y, seen on top of STM32MP257 package) you have ?
Regards.
2024-08-06 10:08 PM
Hi @PatrickF
Thank you for your reply.
Please find the details of the board below:
Note that the STM32MP257F-EV1 board has a sticker with "ES" on it.
Thank you, I understand that CubeProgrammer cannot be used via ST-LINK to debug and can only be used to flash images. We will try to use STM32CubeIDE instead via ST-LINK(SWD).
Since you are able to perform debug by connecting Lauterbach Trace32 PowerDebug via the MIPI10 connector (CN22) of the STM32MP257F-EV1, could you please let me know if there is any procedure to be followed (jumper, boot mode etc.) when Lauterbach debugger is used.
We thought that when the board is booted using 'Development boot', JTAG (DAP) would be enabled. But unfortunately access is denied.
I would appreciate any help with regard to this.
Thank you again.
2024-08-06 11:42 PM
Hi,
in 'development boot' (BOOT=0b0011 or 0b1100), the debug is enabled and nothing specific is needed to access thru JTAG/SWD. In development boot, the red led (LD1, close to reset button) is light.
As you are building debuggers for ST chipset, There is maybe some partnership already in place. Could you give me more details on your company and if you get the board through distributor or directly from ST (by private message if you prefer).
If it helps, here is part of the T32 initialisation I use:
SYStem.RESetOut
wait 100.ms
; Cortex-A35
sys.cpu CortexA35
; JTAG/SWD freq
system.JTAGCLOCK 2M
SYSTEM.CONFIG.DEBUGPORTTYPE SWD
SYStem.CONFIG SWDP ON
; DAP Config
sys.config CHIPIRPRE 4.
sys.config CHIPDRPRE 1.
sys.config DAPIRPOST 5.
sys.config DAPDRPOST 1.
; Dual core (A35)
system.CONFIG.CoreNumber 2.
;Assign the two CA35 to this debug session
core.assign 1. 2.
; Debug base address for each core
SYStem.CONFIG.COREDEBUG.Base DAP:0x80210000 DAP:0x80310000
; Config access ports
SYStem.CONFIG MEMORYACCESSPORT 0.
SYStem.CONFIG AHBACCESSPORT 0.
SYStem.CONFIG APBACCESSPORT 0.
SYStem.CONFIG DEBUGACCESSPORT 0.
SYStem.CONFIG AXIACCESSPORT 4.
sys.o.WaitReset 1.s
sys.o.EnReset OFF
sys.o.ResBreak OFF
; connect DAP only
SYStem.Mode.Prepare
; Disable vector catch
tronchip.reset
tronchip.set reset off
tronchip.set StepVector off
; Attach and halt
sys.mode.up
if run()
break.
I you cannot progress, maybe ask for direct support to your local ST representative.
Regards.
2024-08-07 10:45 PM
Hi @PatrickF
Thank you for your detailed reply again.
Using the T32 information provided by you, we were able to access the chip. The JTAG clock set was different in our case. and we were able to access the chip when the clock was set to 20MHz.
I apprecaite your timely response.
Thank you again.