Skip to main content
gaurav
Associate
May 16, 2024
Question

Wireless Peer to Peer communication w/o user intervention pairing

I'm trying to find out the wireless technology that I can use for peer to peer communication. The main requirement is to have good data transfer speed (at least 500kps or more), pairing process should be without user intervention and the devices will be in close proximity during the communication, probably <15cm.
I have evaluated UWB but it seems packet loss could be an issue there. IR is out as well due to speed and longevity. Do you think active NFC will fit into my need?
I understand that BLE and WiFi Direct could be another option but those will demand another technology for without user intervention pairing. Any thoughts are highly appreciated?

This topic has been closed for replies.

3 replies

Andrew Neil
Super User
May 16, 2024

BLE doesn't require pairing - you can have the Central just connect as soon as it sees the advertising from your device.

Maybe some proprietary 2.4GHz ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
gaurav
gauravAuthor
Associate
May 17, 2024

Thank you for your response Andrew!

There could be multiple peripheral devices in vicinity, central device need to know which one to communicate. So even with Just Work pairing you will still need some human intervention for selecting the right peripheral or need to rely on other tech like NFC or something else, which is not desired. 

Can you please shed some more light on proprietary 2.4GHz?

Andrew Neil
Super User
May 17, 2024

@gaurav wrote:

There could be multiple peripheral devices in vicinity, central device need to know which one to communicate.


Of course: that's fundamental - irrespective of what comms protocol you use!

Unless you just have it connect to every valid device it can "see" - which is what NFC does.

 


@gaurav wrote:

Can you please shed some more light on proprietary 2.4GHz?


AndrewNeil_0-1715938054581.png

 

"Proprietary" means you can make up anything you like from scratch!

The possibilities are endless!

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.