2023-12-18 7:42 PM - edited 2023-12-18 7:43 PM
HI,All
I noticed that when we use BLE stack, we must set SYSCLK to 16MHz。When i set the SYSCLK upto 100MHz,the uart1 log will be garbled after call BleStack_Init which contained in st ble stack lib。I don't know if my discovery is correct。I don't understand why ST doesn't provide the source code for the Bluetooth protocol stack。
Solved! Go to Solution.
2024-01-08 1:04 AM
Hell again @Xiaojie
The maximum SYSCLK is 100MHz for voltage scaling range 1 and 16Mhz for voltage scaling range 2:
So, to be able to have a SYSCLK up to 100MHz, you need to change the voltage scaling range from 2 to 1:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-05 7:17 AM
Hello @Xiaojie
For the UART problem, I think is related to the Baud rate or other UART configurations.
For the examples, You can take a look at the examples using NUCLEO-WBA55CG.
And you can adapt them to the STM32WBA52CG.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-07 11:38 PM - edited 2024-01-07 11:49 PM
Hi,
Thank you for your replay.
I open a ble_beacon project in STM32Cube_FW_WBA_V1.2.0 which adapted for NUCLEO-WBA55CG。
The default SYSCLK and HCLK1 is 16MHz, when i changed the System Clock Mux to PLLCLK, Then SYSCLK is up to 64MHz,the STM32CubeMX noticed me that the System Clock must be <= 16MHz。
Why the STM32CubeMX noticed this error?
Thanks
2024-01-08 1:04 AM
Hell again @Xiaojie
The maximum SYSCLK is 100MHz for voltage scaling range 1 and 16Mhz for voltage scaling range 2:
So, to be able to have a SYSCLK up to 100MHz, you need to change the voltage scaling range from 2 to 1:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-08 2:09 AM
Thank you very much!!
2024-04-27 7:22 PM - edited 2024-04-27 7:42 PM
HI,
I notify that the ble stack will modify the RCC configuration。You can see my another issue:
https://community.st.com/t5/stm32-mcus-wireless/ble-stack-modify-the-rcc-configuration/td-p/667539
So if we choose SYSCLK or PCLK2 as usart clock and init the usart befor calling BleStack_Init, the frequency of usart clock will change after calling BleStack_Init. Then the usart will be garbled.
Thanks