2019-06-06 06:39 AM
In my code i try to delete a flash mem page using
if(HAL_FLASHEx_Erase(&FlashErase,&PageError) != HAL_OK)
but always got an HAL_ERROR because in this function (which is called in HAL_FLASHEx_Erase...)
HAL_StatusTypeDef FLASH_WaitForLastOperation(uint32_t Timeout)
{
uint32_t error;
uint32_t tickstart = HAL_GetTick();
/* Wait for the FLASH operation to complete by polling on BUSY flag to be reset.
Even if the FLASH operation fails, the BUSY flag will be reset and an error
flag will be set */
while (__HAL_FLASH_GET_FLAG(FLASH_FLAG_BSY))
{
if ((HAL_GetTick() - tickstart) >= Timeout)
{
return HAL_TIMEOUT;
}
}
/* check flash errors. Only ECC correction can be checeked here as ECCD
generates NMI */
error = FLASH->SR;
/* Check FLASH End of Operation flag */
if ((error & FLASH_FLAG_EOP) != 0U)
{
/* Clear FLASH End of Operation pending bit */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP);
}
/* Now update error variable to only error value */
error &= FLASH_FLAG_SR_ERROR;
/* Update error with ECC error value */
error |= (FLASH->ECCR & FLASH_FLAG_ECCC);
/* clear error flags */
__HAL_FLASH_CLEAR_FLAG(error);
if (error != 0U)
{
/*Save the error code*/
pFlash.ErrorCode = error;
return HAL_ERROR;
}
/* Wait for control register to be written */
while (__HAL_FLASH_GET_FLAG(FLASH_FLAG_CFGBSY))
{
if ((HAL_GetTick() - tickstart) >= Timeout)
{
return HAL_TIMEOUT;
}
}
error = FLASH->SR sets error to 0x8000.
In the datasheet this part is marked as reserved so why FLASH-SR sets this error bit and blocks the erase process?
Thank you all for your comments!
Solved! Go to Solution.
2019-06-07 02:49 AM
With those details, i can reproduce your issue with the exact same board only P-NUCLEO-WB55 / EPNWB55$CU4. This cannot be observed on the official P-NUCLEO-WB55 kit.
Those EPNWB55$CU4 are not supported inside the STM32CubeFWWB. Especially, you cannot change the BLE stack at all with the one provided. For this reason, i cannot plan any change iniside the HAL FLASH driver to handle this situation.
You can use this workaround to erase your flash with this specific board:
/* USER CODE BEGIN 1 */
/* + Workaround: Engineering samples with FLASH_SR_OPTVERR bit set for P-NUCLEO-WB55 / EPNWB55$CU4 */
/* /!\ This can be apply ONLY to those Engineering samples /!\ */
/* Reset FLASH_SR_OPTVERR bit by software at each startup */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
/* - Workaround: Engineering samples with FLASH_SR_OPTVERR bit set for P-NUCLEO-WB55 / EPNWB55$CU4 */
/* USER CODE END 1 */
With this workaround, your above code behave as expected.
Pierre.
2019-06-06 11:54 PM
Hi Fabsch,
The error you mention is related to FLASH SR: Bit 15 OPTVERR: Option and Engineering bits loading validity error.
Can you describe your setup and boards (value of the sticker at the bottom of the board)?
Did you change the option bytes using STM32CubeProgrammer (associated version?) or any other method?
Did you make any action which can change the option bytes?
BR.
2019-06-07 12:09 AM
Hi Pierre,
Thank you for your answer. I am using a P-NUCLEO-WB55 / EPNWB55$CU4.
With the used software:
CubeIDE
Version: 1.0.0
Build: 2872_20190423-2022 (UTC)
STM32CubeMX - STM32 Device Configuration Tool
Version: 5.2.0
Build: 20190423-0831 (UTC)
I Created a new projekt with IDE and MX Cube for the preconfigured Board. In the Board selector I choose P-NUCLEO-WB55-Nucleo
In the generated code i add following lines of coded:
/* USER CODE BEGIN WHILE */
FLASH_EraseInitTypeDef FlashErase;
FlashErase.NbPages = 1;
FlashErase.Page = 254;
FlashErase.TypeErase = TYPEERASE_PAGES;
uint32_t PageError = 0;
//------------------working delete procedure
// HAL_FLASH_Unlock();
// __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGSERR | FLASH_FLAG_PGAERR);
// /* Process Locked */
// __HAL_LOCK(&pFlash);
// FLASH_PageErase(255);
// /* Process Unlocked */
// __HAL_UNLOCK(&pFlash);
//------------------delete end
//Not working because of error = 0x8000
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGSERR | FLASH_FLAG_PGAERR);
if(HAL_FLASHEx_Erase(&FlashErase,&PageError) != HAL_OK){
HAL_GPIO_WritePin(GPIOB, LD3_Pin, GPIO_PIN_SET); // indicator for erasing fails
}
LED indicates that the error occurred and in the memory viewer that the flash memory is not erased.
With this part the flash memory can erased without problems:
//------------------working delete procedure
// HAL_FLASH_Unlock();
// __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGSERR | FLASH_FLAG_PGAERR);
// /* Process Locked */
// __HAL_LOCK(&pFlash);
// FLASH_PageErase(255);
// /* Process Unlocked */
// __HAL_UNLOCK(&pFlash);
//------------------delete end
Thank you!
2019-06-07 12:21 AM
Ok, Those are engineering sample (ES).
Can you tell us the workshop date and location where you get this sample. This is an important information to know the software compatibilities with those ES.
(also your previous response has been truncated)
STM32CubeFW version used?
Did you change the BLE stack or the FUS?
2019-06-07 12:28 AM
Got this sample at ST workshop in Hamburg at the 29.01.2019.
2019-06-07 12:30 AM
With the used software:
CubeIDE
Version: 1.0.0
Build: 2872_20190423-2022 (UTC)
STM32CubeMX - STM32 Device Configuration Tool
Version: 5.2.0
Build: 20190423-0831 (UTC)
I Created a new projekt with IDE and MX Cube for the preconfigured Board. In the Board selector I choose P-NUCLEO-WB55-Nucleo
In the generated code i add following lines of coded:
/* USER CODE BEGIN WHILE */
FLASH_EraseInitTypeDef FlashErase;
FlashErase.NbPages = 1;
FlashErase.Page = 254;
FlashErase.TypeErase = TYPEERASE_PAGES;
uint32_t PageError = 0;
//------------------working delete procedure
// HAL_FLASH_Unlock();
// __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGSERR | FLASH_FLAG_PGAERR);
// /* Process Locked */
// __HAL_LOCK(&pFlash);
// FLASH_PageErase(255);
// /* Process Unlocked */
// __HAL_UNLOCK(&pFlash);
//------------------delete end
//Not working because of error = 0x8000
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGSERR | FLASH_FLAG_PGAERR);
if(HAL_FLASHEx_Erase(&FlashErase,&PageError) != HAL_OK){
HAL_GPIO_WritePin(GPIOB, LD3_Pin, GPIO_PIN_SET); // indicator for erasing fails
}
I only added these lines of code no changes done after MX Cube created the code. (Used standard configuration after installation of MxCubeIDE and MxCubeCodeconfigurator)
2019-06-07 02:49 AM
With those details, i can reproduce your issue with the exact same board only P-NUCLEO-WB55 / EPNWB55$CU4. This cannot be observed on the official P-NUCLEO-WB55 kit.
Those EPNWB55$CU4 are not supported inside the STM32CubeFWWB. Especially, you cannot change the BLE stack at all with the one provided. For this reason, i cannot plan any change iniside the HAL FLASH driver to handle this situation.
You can use this workaround to erase your flash with this specific board:
/* USER CODE BEGIN 1 */
/* + Workaround: Engineering samples with FLASH_SR_OPTVERR bit set for P-NUCLEO-WB55 / EPNWB55$CU4 */
/* /!\ This can be apply ONLY to those Engineering samples /!\ */
/* Reset FLASH_SR_OPTVERR bit by software at each startup */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
/* - Workaround: Engineering samples with FLASH_SR_OPTVERR bit set for P-NUCLEO-WB55 / EPNWB55$CU4 */
/* USER CODE END 1 */
With this workaround, your above code behave as expected.
Pierre.
2019-06-07 02:56 AM
Works for me. Thank you!
2020-07-29 12:48 AM
Hey Pierre,
I bought a few STM32WB55CG and put them in my custom board. I have the same problem as described here: the fucntion
HAL_FLASHEx_Erase(&FlashErase,&PageError)
returns an error because "error = FLASH->SR" sets error to "0x8000"
I copy/pasted the workaround you posted:
/* USER CODE BEGIN 1 */
/* + Workaround: Engineering samples with FLASH_SR_OPTVERR bit set for P-NUCLEO-WB55 / EPNWB55$CU4 */
/* /!\ This can be apply ONLY to those Engineering samples /!\ */
/* Reset FLASH_SR_OPTVERR bit by software at each startup */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
/* - Workaround: Engineering samples with FLASH_SR_OPTVERR bit set for P-NUCLEO-WB55 / EPNWB55$CU4 */
/* USER CODE END 1 */
And everything runs smoothly.
Could you enlighten me on why do I meet this problem? Do I have one of these engeneering sample?
Cheers,
2020-07-29 02:40 AM
Hello @XP.1oncet ,
As inside the initial thread, can you indicate where did you acquire your part and the exact marking on them.
Additionnaly, which STM32Cube Firmware Package version are you using?
Other tools versions like the STM32CubeProgrammer, STM32CubeIDE?
Did you flash any wireless stack or change the option bytes ?
The observed behavior occurs while using the examples projects from the STM32Cube Firmware Package?
All the aboves informations are important to understand the option byte behavior.
BR.
Pierre.