cancel
Showing results for 
Search instead for 
Did you mean: 

which example project/ video tutorial for sending data to a stm32wb55rg nucleo via python & BLE

MK..1
Associate III

Hi

I need to send (and possbly receive) data via BLE and python to a Stm32wb55RG Nucleo board. THere are so many examples. Which one should I Take or which one is best suited for me as a starting point?

I am trying not to watch 100s of videos. Or Do I need to watch them all? ;)

2 REPLIES 2

Perhaps get a file manager, or grep the sources to narrow things down a little

Or team up with similarly motivated members

https://community.st.com/s/question/0D53W00001qJ8YKSA0/stm32wb-nucleo-please-share-an-example-to-send-data-from-stm-to-the-computer-via-ble

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Sarra.S
ST Employee

Hello @MK..1​ and welcome to the community 

You can start with this link:

public/stm32python/bluetooth-low-energy/nucleo-wb55 · master · STM32 Python / assets · GitLab

I have to mention that some concerned scripts are still under development, thus, if u have any problem, you can mention it here.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.