2022-09-24 2:13 PM
Calling "aci_gap_additional_beacon_start" first works successfully, but calling "aci_gap_set_discoverable" after that returns "0x0C Command disallowed".
If I swap these instructions and set up the main advertisement first, I get the same 0x0C error trying to set up an additional beacon.
Please find the code example here: https://github.com/flipperdevices/flipperzero-firmware/blob/zlo/additional_beacon_test/firmware/targets/f7/ble_glue/gap.c
Main advertisement initialization is contained in the "gap_advertise_start" function. Beacon initialization is inside "beacon_start".
Radiostack versions used: 1.13.3 Lite, 1.14.1 Lite
Solved! Go to Solution.
2022-10-12 7:56 AM
Hello,
I checked your code and I think I found the root cause of your issue, to support advertising and additional beaconing feature, you should have at least to support 2 links. To do this, change the value of the following define in app_conf.h file:
#define CFG_BLE_NUM_LINK 2Best Regards
2022-09-25 5:50 AM
Update: I also tried 1.14.1 Lite, but no luck.
2022-10-07 8:55 AM
Hello,
Are you using P-NUCLEO-WB55 Nucleo board or a custom board? Did you try to start from an example of STM32CubeWB package for example BLE_p2pServer?
Best Regards
2022-10-07 9:00 AM
Hi @Remy ISSALYS!
I am using a custom board, namely a Flipper Zero device. Unfortunately, I don't have a Nucleo board, and I'm not experienced enough to compile bare BLE_p2pServer for Flipper Zero.
However, all BLE advertising initialization code can be found here, including the attempt to use additional beacon: https://github.com/flipperdevices/flipperzero-firmware/blob/zlo/additional_beacon_test/firmware/targets/f7/ble_glue/gap.c
2022-10-12 7:56 AM
Hello,
I checked your code and I think I found the root cause of your issue, to support advertising and additional beaconing feature, you should have at least to support 2 links. To do this, change the value of the following define in app_conf.h file:
#define CFG_BLE_NUM_LINK 2Best Regards
2022-10-12 8:09 AM
Thank you, Remy, this helped.