2025-02-06 03:16 AM - last edited on 2025-02-06 03:20 AM by Andrew Neil
Moved from MPUs forum.
Hi,
I looking to use the Nucleo WB55RG board to prototype some BLE firmware.
I was looking through the examples in Cube MX but that particular board wasn't listed but there were a few similar choices, (see below). I was thinking the NUCLEO-WBAA55CG or the P-NUCLEO-WB55-NUCLEO?
Solved! Go to Solution.
2025-02-06 03:18 AM
Hello @NicRoberts
To use the Nucleo-WB55RG you should select the P-NUCLEO-WB55-NUCLEO.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-06 03:18 AM
Hello @NicRoberts
To use the Nucleo-WB55RG you should select the P-NUCLEO-WB55-NUCLEO.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-06 03:19 AM
What CubeMX version are you using?
You posted this in the MPUs section, so are you sure you're using the correct CubeMX version - one for MCUs ?