2021-10-30 4:31 PM
I am using hw_timerserver and sequencer for BLE. I added additional tasks to the sequencer for my application. It appeared that my tasks are running much too frequently, so I looked into the clock configuration of the RTC and found that WUCLK was driven by HSE and did not have the WU Clock and WU Counters configured properly. I switched the clock source to LSE, with WU clock & counters set to RTCCLK/16 & 2, for proper operation in Low-power modes. I then found that Systick was slowed down considerably. Any ideas?
2021-11-01 7:33 PM
2021-11-23 10:41 AM
Hello,
There is clearly no connection between RTCCLK and Systick.
I would check the configuration of the Systick. For an unknown reason, I believe it has been wrongly setup.
Regards.